<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: WDI PIN OF PF8100 TO LS1046</title>
    <link>https://community.nxp.com/t5/Layerscape/WDI-PIN-OF-PF8100-TO-LS1046/m-p/1478792#M10739</link>
    <description>&lt;P&gt;&lt;SPAN&gt;To enable WD reset, connect the pin to HRESET of LS1046A.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Required input assertion time of HRESET_B is 32 SYSCLKs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Customer has to keep in mind the following when enabling WD reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. If min. assertion time of WD pin is greater than min. assertion time of HRESET then WD reset will be successful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. If WD reset is configurable then change the min assertion time of WDI pin as per the requirement based on HRESET. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. If WD reset is not configurable the use Reset IC in between.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Jun 2022 06:57:00 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-06-23T06:57:00Z</dc:date>
    <item>
      <title>WDI PIN OF PF8100 TO LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/WDI-PIN-OF-PF8100-TO-LS1046/m-p/1476334#M10719</link>
      <description>&lt;P&gt;To which pin of LS1046 I should connect WDI pin of PF8100 PMIC, if I want to enable WD reset?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please find PF8100 datasheet.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jun 2022 00:24:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/WDI-PIN-OF-PF8100-TO-LS1046/m-p/1476334#M10719</guid>
      <dc:creator>Ellu24</dc:creator>
      <dc:date>2022-06-20T00:24:33Z</dc:date>
    </item>
    <item>
      <title>Re: WDI PIN OF PF8100 TO LS1046</title>
      <link>https://community.nxp.com/t5/Layerscape/WDI-PIN-OF-PF8100-TO-LS1046/m-p/1478792#M10739</link>
      <description>&lt;P&gt;&lt;SPAN&gt;To enable WD reset, connect the pin to HRESET of LS1046A.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Required input assertion time of HRESET_B is 32 SYSCLKs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Customer has to keep in mind the following when enabling WD reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. If min. assertion time of WD pin is greater than min. assertion time of HRESET then WD reset will be successful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. If WD reset is configurable then change the min assertion time of WDI pin as per the requirement based on HRESET. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. If WD reset is not configurable the use Reset IC in between.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 06:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/WDI-PIN-OF-PF8100-TO-LS1046/m-p/1478792#M10739</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-23T06:57:00Z</dc:date>
    </item>
  </channel>
</rss>