<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is the DPL content a device tree file? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Is-the-DPL-content-a-device-tree-file/m-p/1476035#M10716</link>
    <description>&lt;P&gt;Yes, this is for configuring the mc. Note that both dpc adn dpl need to be configured correctly.&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jun 2022 13:15:17 GMT</pubDate>
    <dc:creator>kenli</dc:creator>
    <dc:date>2022-06-17T13:15:17Z</dc:date>
    <item>
      <title>Is the DPL content a device tree file?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-the-DPL-content-a-device-tree-file/m-p/1473375#M10677</link>
      <description>&lt;P&gt;I'm using LX2160ardb_rev2&lt;/P&gt;&lt;P&gt;Originally, there is no Ethernet driver for the LX2160 in linux, but when booting ubuntu from uboot, the Ethernet driver is enabled in ubuntu by sf reading the DPL file and then setting the boot configuration with fsl_mc.&lt;/P&gt;&lt;P&gt;I believe the entity of this DPL file is "dpl-eth.19.dtb", is this correct?&lt;/P&gt;&lt;P&gt;And if so, is it correct to recognize that DPL file = DTB file?&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 06:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-the-DPL-content-a-device-tree-file/m-p/1473375#M10677</guid>
      <dc:creator>m_kei</dc:creator>
      <dc:date>2022-06-14T06:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: Is the DPL content a device tree file?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-the-DPL-content-a-device-tree-file/m-p/1476035#M10716</link>
      <description>&lt;P&gt;Yes, this is for configuring the mc. Note that both dpc adn dpl need to be configured correctly.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 13:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-the-DPL-content-a-device-tree-file/m-p/1476035#M10716</guid>
      <dc:creator>kenli</dc:creator>
      <dc:date>2022-06-17T13:15:17Z</dc:date>
    </item>
  </channel>
</rss>