<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: eth0 is always up during bootup</title>
    <link>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1475841#M10713</link>
    <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Thanks for the support actually the netplan configuration was creating the issue. So we removed it during the build and flashed the board and we are not observing the eth0 interface up.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jun 2022 08:31:05 GMT</pubDate>
    <dc:creator>deepanrajanbara</dc:creator>
    <dc:date>2022-06-17T08:31:05Z</dc:date>
    <item>
      <title>eth0 is always up during bootup</title>
      <link>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1471974#M10660</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Hi,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;In our custom board we are using dpmac3,dpmac4 and dpmac17. According to our dpl configuration only dpmac17 is added and it is working fine. But what we want is during bootup we observe that always our dpmac17 is running dhcp and getting IP address. we wanted dpmac17 to be added but it should be in down state. How do we do this setting in our BSP. Please let us know ASAP.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jun 2022 04:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1471974#M10660</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2022-06-10T04:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: eth0 is always up during bootup</title>
      <link>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1474360#M10693</link>
      <description>&lt;P&gt;Do you use LSDK now?&lt;/P&gt;
&lt;P&gt;Did you modify&amp;nbsp;/etc/network/interfaces to configure eth0?&lt;/P&gt;
&lt;P&gt;Would you please provide your Linux Kernel booting up log?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 10:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1474360#M10693</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-15T10:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: eth0 is always up during bootup</title>
      <link>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1475841#M10713</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Thanks for the support actually the netplan configuration was creating the issue. So we removed it during the build and flashed the board and we are not observing the eth0 interface up.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Deepanraj.A&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jun 2022 08:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/eth0-is-always-up-during-bootup/m-p/1475841#M10713</guid>
      <dc:creator>deepanrajanbara</dc:creator>
      <dc:date>2022-06-17T08:31:05Z</dc:date>
    </item>
  </channel>
</rss>