<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OpenWRT on LS1046A-RDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1474719#M10697</link>
    <description>&lt;P&gt;Something to note, I did compare the ddr_init.c and platform_def.h files in the OpenWRT repo vs the flexbuild NXP Ubuntu repo and did confirm that the files in OpenWRT are older and have some significant changes.&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 20:21:14 GMT</pubDate>
    <dc:creator>rapter465</dc:creator>
    <dc:date>2022-06-15T20:21:14Z</dc:date>
    <item>
      <title>OpenWRT on LS1046A-RDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1474716#M10696</link>
      <description>&lt;P&gt;I am currently evaluating a new LS1046A-RDB board for consideration in our next product. We are working through getting the different LSDKs loaded into QSPI and eMMC with mixed success. While we've been able to flash and boot to the Ubuntu-based LSDK, we are currently unable to flash and boot from either QSPI, eMMC, or SD Card for OpenWRT. I've tried both upstream latest stable OpenWRT (v21.02.3), as well as the Layerscape 20.09 fork. Attempting to boot either builds (as well as reference build from OpenWRT's website) results in the following error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//////////////////////////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;NOTICE: UDIMM 18ADF2G72AZ-2G6E1&lt;BR /&gt;ERROR: Board parameters no match.&lt;BR /&gt;ERROR: Failed matching board timing.&lt;BR /&gt;ERROR: Found training error(s): 0x2100&lt;BR /&gt;ERROR: Error: Waiting for D_INIT timeout.&lt;BR /&gt;ERROR: Writing DDR register(s) failed&lt;BR /&gt;ERROR: Programing DDRC error&lt;BR /&gt;ERROR: DDR init failed.&lt;BR /&gt;NOTICE: Incorrect DRAM0 size is defined in platfor_def.h&lt;BR /&gt;ERROR: mmap_add_region_check() failed. error -22&lt;BR /&gt;ERROR: mmap_add_region_check() failed. error -22&lt;BR /&gt;NOTICE: BL2: v1.5(release):layerscape-20.09&lt;BR /&gt;NOTICE: BL2: Built : 03:57:39, Sep 24 2020&lt;BR /&gt;ERROR: SD read error - DMA error = 10000000&lt;BR /&gt;ERROR: Read error = fffffffb&lt;BR /&gt;ERROR: BL2: Failed to load image (-2)&lt;BR /&gt;Authentication failure&lt;/P&gt;&lt;P&gt;//////////////////////////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I built OpenWRT with the following menuconfig options:&lt;/P&gt;&lt;P&gt;./scripts/feeds update -a&lt;BR /&gt;./scripts/feeds install -a&lt;/P&gt;&lt;P&gt;make defconfig&lt;BR /&gt;make menuconfig&lt;BR /&gt;- Target System: NXP Layerscape&lt;BR /&gt;- Subtarget: ARMv8 64-bit based boards&lt;BR /&gt;- Target Profile: NXP LS1046A-RDB SD Card Boot&lt;/P&gt;&lt;P&gt;make -j1 V=s&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any assistance would be greatly appreciate as we work through our trade study.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 20:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1474716#M10696</guid>
      <dc:creator>rapter465</dc:creator>
      <dc:date>2022-06-15T20:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: OpenWRT on LS1046A-RDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1474719#M10697</link>
      <description>&lt;P&gt;Something to note, I did compare the ddr_init.c and platform_def.h files in the OpenWRT repo vs the flexbuild NXP Ubuntu repo and did confirm that the files in OpenWRT are older and have some significant changes.&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 20:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1474719#M10697</guid>
      <dc:creator>rapter465</dc:creator>
      <dc:date>2022-06-15T20:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: OpenWRT on LS1046A-RDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1489189#M10873</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please put the attached patch in folder&amp;nbsp;openwrt/package/boot/tfa-layerscape/patches, then run "make" to rebuild image.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jul 2022 05:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OpenWRT-on-LS1046A-RDB/m-p/1489189#M10873</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-07-14T05:57:09Z</dc:date>
    </item>
  </channel>
</rss>