<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: CodeWarrior / TAP / LS1046ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1474048#M10685</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Please refer to section "3.2 Working with bareboard application" in&amp;nbsp;C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf to create a bareboard project in CodeWarrior IDE to connect to the target board.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 03:58:13 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-06-15T03:58:13Z</dc:date>
    <item>
      <title>CodeWarrior / TAP / LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1473160#M10676</link>
      <description>&lt;P&gt;I cannot connect to my TAP module from CodeWarrior.&amp;nbsp; I am receive a "Problem Occurred" pop-up window that states 'Launching LS1046A_RDB(1)_Connect' has encountered a problem.&amp;nbsp; Program file not specified.&amp;nbsp; This occurs when I use the flash icon in the Target Connection Configuration window.&lt;/P&gt;&lt;P&gt;Any pointers would be very appreciated.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 21:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1473160#M10676</guid>
      <dc:creator>Daves_Garage</dc:creator>
      <dc:date>2022-06-13T21:58:10Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior / TAP / LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1474048#M10685</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please refer to section "3.2 Working with bareboard application" in&amp;nbsp;C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf to create a bareboard project in CodeWarrior IDE to connect to the target board.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 03:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1474048#M10685</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-15T03:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior / TAP / LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1475396#M10709</link>
      <description>&lt;P&gt;A more detailed description of the issue can be found here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape/LS1046ARDB-and-using-CodeWarrior-to-reflash-QSPI-flash-with/m-p/1474056/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufEw0RjJPQlBRTzNSMDRFfDE0NzQwNTZ8U1VCU0NSSVBUSU9OU3xoSw#M10686" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/LS1046ARDB-and-using-CodeWarrior-to-reflash-QSPI-flash-with/m-p/1474056/emcs_t/S2h8ZW1haWx8dG9waWNfc3Vic2NyaXB0aW9ufEw0RjJPQlBRTzNSMDRFfDE0NzQwNTZ8U1VCU0NSSVBUSU9OU3xoSw#M10686&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jun 2022 15:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CodeWarrior-TAP-LS1046ARDB/m-p/1475396#M10709</guid>
      <dc:creator>Daves_Garage</dc:creator>
      <dc:date>2022-06-16T15:27:03Z</dc:date>
    </item>
  </channel>
</rss>