<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1023A in 16-bit data bus width configuration</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1474035#M10684</link>
    <description>&lt;P&gt;&lt;SPAN&gt;if the DDR_SDRAM_CFG[DBW] = 2'b10 for 16-bit data bus configuration, the MDQ [0:15] will be used. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if the DDR_SDRAM_CFG[DBW] = 2'b01 for 32-bit data bus configuration, the MDQ [0:31] will be used.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 03:26:27 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-06-15T03:26:27Z</dc:date>
    <item>
      <title>LS1023A in 16-bit data bus width configuration</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1468745#M10626</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;We are designing a custom board based on a LS1023A with 2GB DDR4 + ECC (one bank).&lt;BR /&gt;We plan to connect and use this DDR memory with a 16-bit data bus witdh.&lt;BR /&gt;It seems to be OK by adjusting&amp;nbsp;DDR_SDRAM_CFG[DBW] to '10b' as mentioned in the Reference Manual.&lt;BR /&gt;However, it is not clearly noted which data bus lanes we must use in this case : MDQ[15..0] or MDQ[31..16] ?&lt;BR /&gt;Regards,&lt;/P&gt;&lt;P&gt;Samuel&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jun 2022 13:35:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1468745#M10626</guid>
      <dc:creator>SamCo</dc:creator>
      <dc:date>2022-06-03T13:35:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1023A in 16-bit data bus width configuration</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1473659#M10680</link>
      <description>&lt;P&gt;The DDR data assignment of the bus data is proposed into document Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces, Rev. 2, 07/2019 page 4&amp;nbsp; Table 1. DDR4 design checklist (continued).&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5097" target="_blank"&gt;AN5097, Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces - Application Note&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Route all signals within a given byte lane on the same critical layer with the same via&lt;/P&gt;
&lt;P&gt;count. Assuming ECC is used, the DDR4 data bus consists of nine data byte lanes.&lt;/P&gt;
&lt;P&gt;NOTE: The byte ordering below is not a requirement; byte lanes can be routed in the&lt;/P&gt;
&lt;P&gt;order that best fits the customer design.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Byte lane 0—MDQ(7:0), MDM(0), MDQS(0), MDQS(0)&lt;/LI&gt;
&lt;LI&gt;Byte lane 1—MDQ(15:8), MDM(1), MDQS(1), MDQS(1)&lt;/LI&gt;
&lt;LI&gt;Byte lane 2—MDQ(23:16), MDM(2), MDQS(2), MDQS(2)&lt;/LI&gt;
&lt;LI&gt;Byte lane 3—MDQ(31:24), MDM(3), MDQS(3), MDQS(3)&lt;/LI&gt;
&lt;LI&gt;Byte lane 4—MDQ(39:32), MDM(4), MDQS(4), MDQS(4)&lt;/LI&gt;
&lt;LI&gt;Byte lane 5—MDQ(47:40), MDM(5), MDQS(5), MDQS(5)&lt;/LI&gt;
&lt;LI&gt;Byte lane 6—MDQ(55:48), MDM(6), MDQS(6), MDQS(6)&lt;/LI&gt;
&lt;LI&gt;Byte lane 7—MDQ(63:56), MDM(7), MDQS(7), MDQS(7)&lt;/LI&gt;
&lt;LI&gt;Byte lane 8—MECC(7:0), MDM(8), MDQS(8), MDQS(8)&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;To facilitate fan-out of the DDR4 data lanes (if needed), alternate adjacent data lanes&lt;/P&gt;
&lt;P&gt;onto different critical layers (see Figure 1 and Figure 2).&lt;/P&gt;
&lt;P&gt;NOTE: Some product implementations may only implement a 32-bit wide interface.&lt;/P&gt;
&lt;P&gt;NOTE: If the device supports ECC, NXP highly recommends that the user implements&lt;/P&gt;
&lt;P&gt;ECC on the initial hardware prototypes.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Additional information is proposed o application note QorIQ LS1043A Design Checklist , Rev. 6, 02/2021 page 18 in the note section.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN5012" target="_blank"&gt;AN5012, LS1043A Design Checklist - Application Note&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 13:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1473659#M10680</guid>
      <dc:creator>Pierre_Juste</dc:creator>
      <dc:date>2022-06-14T13:00:18Z</dc:date>
    </item>
    <item>
      <title>Re: LS1023A in 16-bit data bus width configuration</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1474035#M10684</link>
      <description>&lt;P&gt;&lt;SPAN&gt;if the DDR_SDRAM_CFG[DBW] = 2'b10 for 16-bit data bus configuration, the MDQ [0:15] will be used. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if the DDR_SDRAM_CFG[DBW] = 2'b01 for 32-bit data bus configuration, the MDQ [0:31] will be used.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 03:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1023A-in-16-bit-data-bus-width-configuration/m-p/1474035#M10684</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-15T03:26:27Z</dc:date>
    </item>
  </channel>
</rss>