<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1028A RCW generation errors in Code Warrior tool</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-RCW-generation-errors-in-Code-Warrior-tool/m-p/1473489#M10679</link>
    <description>&lt;P&gt;I imported LSDK default RCW file rcw_1500_gpu600.bin in CW 11.5.5, also encountered similar problem as you. There is problem with the CW QCVS tool, please click "Enable/Disable error checking" button to select "Skip error checking". Please refer to the following screenshot.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1655196697468.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183235i9E8F0585C3EA0A8A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="yipingwang_0-1655196697468.png" alt="yipingwang_0-1655196697468.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Jun 2022 08:52:34 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-06-14T08:52:34Z</dc:date>
    <item>
      <title>LS1028A RCW generation errors in Code Warrior tool</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-RCW-generation-errors-in-Code-Warrior-tool/m-p/1472909#M10670</link>
      <description>&lt;P&gt;Dear Experts,&lt;/P&gt;&lt;P&gt;The compiled RCW from the flex build tool path&amp;nbsp;rcw_1500_gpu600.bin&amp;nbsp; (&amp;lt;flexbuild_dir&amp;gt;/packages/firmware/rcw/ls1028ardb/R_SQPP_0x85bb) imported&amp;nbsp;in Codewarrior v11.5.0 and observed some of the required fields having invalid or custom values and tool giving an error when compiling with this.&lt;/P&gt;&lt;P&gt;Error message: PBL image was not generated as it contains error. Fix the problems or check 'ignore constraints' button to generate the PBL image.&lt;/P&gt;&lt;P&gt;As attached an example of RCW error field CGA_PLL1_RAT [31-26] : selected value 0x1111 (a valid value as per processor manual).&lt;/P&gt;&lt;P&gt;Please help!&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jun 2022 13:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-RCW-generation-errors-in-Code-Warrior-tool/m-p/1472909#M10670</guid>
      <dc:creator>kumar_086</dc:creator>
      <dc:date>2022-06-13T13:43:04Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A RCW generation errors in Code Warrior tool</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-RCW-generation-errors-in-Code-Warrior-tool/m-p/1473489#M10679</link>
      <description>&lt;P&gt;I imported LSDK default RCW file rcw_1500_gpu600.bin in CW 11.5.5, also encountered similar problem as you. There is problem with the CW QCVS tool, please click "Enable/Disable error checking" button to select "Skip error checking". Please refer to the following screenshot.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1655196697468.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/183235i9E8F0585C3EA0A8A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="yipingwang_0-1655196697468.png" alt="yipingwang_0-1655196697468.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jun 2022 08:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-RCW-generation-errors-in-Code-Warrior-tool/m-p/1473489#M10679</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-14T08:52:34Z</dc:date>
    </item>
  </channel>
</rss>