<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: Failed to write memory</title>
    <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469583#M10635</link>
    <description>&lt;P&gt;I have the same error with a LA1043A board. Did anyone ever identify the cause of this error and how to work around it?&lt;/P&gt;</description>
    <pubDate>Tue, 07 Jun 2022 00:25:20 GMT</pubDate>
    <dc:creator>richardadams</dc:creator>
    <dc:date>2022-06-07T00:25:20Z</dc:date>
    <item>
      <title>Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1448337#M10440</link>
      <description>&lt;P&gt;I'm getting error via Codewarrior when trying to connect with flash programmer or when I run the initialization script.&lt;/P&gt;&lt;P&gt;Jtag connection seems OK and I am able to read the RCW.&lt;/P&gt;&lt;P&gt;Error is:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;STRONG&gt;Failed to write memory at address 0x2016002c on core CortexA53#0.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;Chip is LS1023A.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;Thanks for your help&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/21537"&gt;@yi&lt;/a&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 09:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1448337#M10440</guid>
      <dc:creator>bladerunner1010</dc:creator>
      <dc:date>2022-04-27T09:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1453720#M10513</link>
      <description>&lt;P&gt;l meet the same question ,how do you solve it&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks you&lt;/P&gt;</description>
      <pubDate>Thu, 05 May 2022 18:18:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1453720#M10513</guid>
      <dc:creator>shu-zyc1</dc:creator>
      <dc:date>2022-05-05T18:18:39Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469583#M10635</link>
      <description>&lt;P&gt;I have the same error with a LA1043A board. Did anyone ever identify the cause of this error and how to work around it?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 00:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469583#M10635</guid>
      <dc:creator>richardadams</dc:creator>
      <dc:date>2022-06-07T00:25:20Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469657#M10637</link>
      <description>&lt;P&gt;please attach your initialization script and will try to help&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 03:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469657#M10637</guid>
      <dc:creator>bladerunner1010</dc:creator>
      <dc:date>2022-06-07T03:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469697#M10639</link>
      <description>&lt;P&gt;I'm using the initialization script for the LS1043ARDB (LS1043A_RDB._init.py) with the following changes to support Hardcoding the RCW since&amp;nbsp; my board has a Blank NOR&amp;nbsp; Flash which will be my boot device when I can program it&lt;/P&gt;&lt;P&gt;USE_SAFE_RCW = True&lt;/P&gt;&lt;P&gt;BOOT_CHIP_SELECT = 2&lt;/P&gt;&lt;P&gt;The error is generated from Init_BRR when the line " DCSR_BE_M(0x16002C, 0x0000000E)" is executed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jun 2022 05:07:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1469697#M10639</guid>
      <dc:creator>richardadams</dc:creator>
      <dc:date>2022-06-07T05:07:29Z</dc:date>
    </item>
    <item>
      <title>回复： Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1988757#M15067</link>
      <description>&lt;P&gt;&lt;SPAN&gt;l meet the same question ,how do you solve it ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 10:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1988757#M15067</guid>
      <dc:creator>weid</dc:creator>
      <dc:date>2024-11-06T10:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to write memory</title>
      <link>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1991001#M15083</link>
      <description>&lt;P&gt;I personally did not, I moved to other projects since then.&lt;BR /&gt;The HW team cont. working on this and then discovered HW issues with the chip's power sequence.&lt;BR /&gt;You need to check that you are not writing to on chip memory so it will falsely show as a write success.&lt;BR /&gt;Also Try to check SPI flash transactions during writes.&lt;BR /&gt;Did you initialize DDR memory properly?&lt;BR /&gt;I think get the power sequence sorted out first, you can use an eval board for reference, I think it is done there using CPLD.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 09:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failed-to-write-memory/m-p/1991001#M15083</guid>
      <dc:creator>bladerunner1010</dc:creator>
      <dc:date>2024-11-08T09:32:41Z</dc:date>
    </item>
  </channel>
</rss>