<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Add Second MMC to LS1021A Device Tree</title>
    <link>https://community.nxp.com/t5/Layerscape/Add-Second-MMC-to-LS1021A-Device-Tree/m-p/1468091#M10618</link>
    <description>&lt;P&gt;LS1021A only has one esdhc controller, it is impossible to use a second MMC.&lt;/P&gt;
&lt;P&gt;You could replace the SD interface with eMMC.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jun 2022 08:15:55 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-06-02T08:15:55Z</dc:date>
    <item>
      <title>Add Second MMC to LS1021A Device Tree</title>
      <link>https://community.nxp.com/t5/Layerscape/Add-Second-MMC-to-LS1021A-Device-Tree/m-p/1451787#M10493</link>
      <description>&lt;P&gt;Hello Everybody,&lt;/P&gt;&lt;P&gt;I would like to add a second eMMC in LS1021A with custom Buildroot Linux image and device tree for a custom board based on LS1021A-IOT board (with additional eMMC, of course).&lt;/P&gt;&lt;P&gt;Using Buildroot I am able to modify and customize the Linux Image.&lt;BR /&gt;&lt;BR /&gt;What is the correct manner for adding additional peripherals?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 May 2022 11:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Add-Second-MMC-to-LS1021A-Device-Tree/m-p/1451787#M10493</guid>
      <dc:creator>Kensou</dc:creator>
      <dc:date>2022-05-02T11:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: Add Second MMC to LS1021A Device Tree</title>
      <link>https://community.nxp.com/t5/Layerscape/Add-Second-MMC-to-LS1021A-Device-Tree/m-p/1468091#M10618</link>
      <description>&lt;P&gt;LS1021A only has one esdhc controller, it is impossible to use a second MMC.&lt;/P&gt;
&lt;P&gt;You could replace the SD interface with eMMC.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jun 2022 08:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Add-Second-MMC-to-LS1021A-Device-Tree/m-p/1468091#M10618</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-02T08:15:55Z</dc:date>
    </item>
  </channel>
</rss>