<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1046ARDB RJ45 UART port reading issue</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1468036#M10617</link>
    <description>&lt;P&gt;Hi Yiping,&lt;/P&gt;&lt;P&gt;We try to install the CP2102 driver already but it appears to get the wrong message.&lt;/P&gt;&lt;P&gt;We then resolve the issue by directly purchase and use RJ45-to-USB cable that suggested from vender.&lt;/P&gt;&lt;P&gt;This case can be close now. Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jun 2022 06:55:27 GMT</pubDate>
    <dc:creator>Chanh</dc:creator>
    <dc:date>2022-06-02T06:55:27Z</dc:date>
    <item>
      <title>LS1046ARDB RJ45 UART port reading issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1456350#M10538</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I change the SW4[4] on my LS1046ARDB board to 0 to use the UART from J4 (using RJ45-to-DB9F cable).&lt;/P&gt;&lt;P&gt;May I know:&lt;/P&gt;&lt;P&gt;1. What is the suggested adapter for this cable to connect to PC, since nowaday the PC will not have com port.&lt;/P&gt;&lt;P&gt;2. What is the pin layout of this 9 pins connector?&lt;/P&gt;&lt;P&gt;3. Since I have a CP2102 USB to UART bridge, I connect it with 9 pin connector. I have set Tera term parameters to be as the getting start guide, but when I reboot the board, I get the garbage message, not the log as in the document. May I know how to resolve it?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 11 May 2022 10:40:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1456350#M10538</guid>
      <dc:creator>Chanh</dc:creator>
      <dc:date>2022-05-11T10:40:19Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB RJ45 UART port reading issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1467968#M10615</link>
      <description>&lt;P&gt;1.&amp;nbsp;&lt;SPAN&gt;The USB2RS232 converter could be used&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. Please refer to "2.11 UART interface" in&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1046ARDBRM" target="_blank" rel="noopener"&gt;&lt;SPAN&gt;LS1046A Reference Design Board Reference Manual&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3. Please remember to install&amp;nbsp;CP2102 driver on your host PC. Please configure serial speed at 115200.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jun 2022 05:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1467968#M10615</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-02T05:23:35Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB RJ45 UART port reading issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1468036#M10617</link>
      <description>&lt;P&gt;Hi Yiping,&lt;/P&gt;&lt;P&gt;We try to install the CP2102 driver already but it appears to get the wrong message.&lt;/P&gt;&lt;P&gt;We then resolve the issue by directly purchase and use RJ45-to-USB cable that suggested from vender.&lt;/P&gt;&lt;P&gt;This case can be close now. Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jun 2022 06:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-UART-port-reading-issue/m-p/1468036#M10617</guid>
      <dc:creator>Chanh</dc:creator>
      <dc:date>2022-06-02T06:55:27Z</dc:date>
    </item>
  </channel>
</rss>