<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックETHERNET CONTROLLER OF LS1046A</title>
    <link>https://community.nxp.com/t5/Layerscape/ETHERNET-CONTROLLER-OF-LS1046A/m-p/1459554#M10553</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am designing a hardware using LS1046 and I want to connect ethernet PHY&amp;nbsp;VSC8502-03 , which uses RGMII MAC interface, so that I have to connect that to EC module of processor. My questions are:&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) what should I connect to EC1_GTX_CLK125 pin( any external crystal or clock generator Si 5332 output or any pins from ethernet PHY)&lt;/P&gt;&lt;P&gt;2)If I am not using EC2 , Can I left it unconnected?&lt;/P&gt;&lt;P&gt;3) Should I use synchronous ethernet as specified in&amp;nbsp;VSC8502-03 datasheet, where should I connect&amp;nbsp;RCVRDCLK1,RCVRDCLK2,&amp;nbsp;CLK_SQUELCH_IN. (I have attached&amp;nbsp;VSC8502-03 datasheet. Please find the attachment)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Tue, 17 May 2022 23:36:45 GMT</pubDate>
    <dc:creator>Ellu24</dc:creator>
    <dc:date>2022-05-17T23:36:45Z</dc:date>
    <item>
      <title>ETHERNET CONTROLLER OF LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/ETHERNET-CONTROLLER-OF-LS1046A/m-p/1459554#M10553</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am designing a hardware using LS1046 and I want to connect ethernet PHY&amp;nbsp;VSC8502-03 , which uses RGMII MAC interface, so that I have to connect that to EC module of processor. My questions are:&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) what should I connect to EC1_GTX_CLK125 pin( any external crystal or clock generator Si 5332 output or any pins from ethernet PHY)&lt;/P&gt;&lt;P&gt;2)If I am not using EC2 , Can I left it unconnected?&lt;/P&gt;&lt;P&gt;3) Should I use synchronous ethernet as specified in&amp;nbsp;VSC8502-03 datasheet, where should I connect&amp;nbsp;RCVRDCLK1,RCVRDCLK2,&amp;nbsp;CLK_SQUELCH_IN. (I have attached&amp;nbsp;VSC8502-03 datasheet. Please find the attachment)&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Tue, 17 May 2022 23:36:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ETHERNET-CONTROLLER-OF-LS1046A/m-p/1459554#M10553</guid>
      <dc:creator>Ellu24</dc:creator>
      <dc:date>2022-05-17T23:36:45Z</dc:date>
    </item>
    <item>
      <title>Re: ETHERNET CONTROLLER OF LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/ETHERNET-CONTROLLER-OF-LS1046A/m-p/1469245#M10633</link>
      <description>&lt;P&gt;Please refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Layerscape/Ethernet-Controller-EC1-GTX-CLK125-pin/td-p/1457572" target="_blank"&gt;https://community.nxp.com/t5/Layerscape/Ethernet-Controller-EC1-GTX-CLK125-pin/td-p/1457572&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jun 2022 08:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ETHERNET-CONTROLLER-OF-LS1046A/m-p/1469245#M10633</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-06T08:47:24Z</dc:date>
    </item>
  </channel>
</rss>