<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCK AND VTT TERMINATION OF DDR4 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/MCK-AND-VTT-TERMINATION-OF-DDR4/m-p/1455981#M10536</link>
    <description>&lt;P&gt;&lt;SPAN&gt;You can use the RDB as a reference. you may also take Micron design rules in consideration. also there is an application note for DDR4 AN5097 that you can use to determine the VTT decoupling caps and more.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 11 May 2022 02:20:55 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-05-11T02:20:55Z</dc:date>
    <item>
      <title>MCK AND VTT TERMINATION OF DDR4</title>
      <link>https://community.nxp.com/t5/Layerscape/MCK-AND-VTT-TERMINATION-OF-DDR4/m-p/1454688#M10517</link>
      <description>&lt;P&gt;I am designing a&amp;nbsp; new hardware using LS1046a.Now I am interfacing ddr4 with processor. I have few doubts regarding the VTT terminations.:&lt;/P&gt;&lt;P&gt;1) Can I use the decoupling capacitors as in attachment (reference board)?&lt;/P&gt;&lt;P&gt;2) or I have to use as specified in micron design rules of decoupling capacitors as: &lt;FONT color="#FF6600"&gt;Use at least one low ESL cap or two standard decoupling caps for each four pack resistor network, Use at least one 4.7 µF cap at each end of the VTT island ,&amp;nbsp;Ensure the VTT island is properly decoupled with bulk decoupling. At least one bulk cap&amp;nbsp;(47–220 µF) capacitor should be at each end of the island.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;3) If it is specified as question 3,the&amp;nbsp; ho the circuit looks like?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;4) which resistor and capacitor to use for MCK termination?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 May 2022 04:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/MCK-AND-VTT-TERMINATION-OF-DDR4/m-p/1454688#M10517</guid>
      <dc:creator>Ellu24</dc:creator>
      <dc:date>2022-05-09T04:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: MCK AND VTT TERMINATION OF DDR4</title>
      <link>https://community.nxp.com/t5/Layerscape/MCK-AND-VTT-TERMINATION-OF-DDR4/m-p/1455981#M10536</link>
      <description>&lt;P&gt;&lt;SPAN&gt;You can use the RDB as a reference. you may also take Micron design rules in consideration. also there is an application note for DDR4 AN5097 that you can use to determine the VTT decoupling caps and more.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 May 2022 02:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/MCK-AND-VTT-TERMINATION-OF-DDR4/m-p/1455981#M10536</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-05-11T02:20:55Z</dc:date>
    </item>
  </channel>
</rss>