<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックGPIO LED support LS1046A</title>
    <link>https://community.nxp.com/t5/Layerscape/GPIO-LED-support-LS1046A/m-p/1451697#M10491</link>
    <description>&lt;P&gt;Hi colleagues,&lt;/P&gt;&lt;P&gt;I am trying to enable LED support via GPIO for our board based on LS1046. In the system I have both mpc8xxx (CONFIG_GPIO_MPC8XXX) based GPIOs and I2C based GPIOs. The LED functionality works for the I2C part e.g.&lt;BR /&gt;echo heartbeat &amp;gt; /sys/class/leds/x1p/trigger&lt;BR /&gt;but for the LS1046 GPIOs&lt;BR /&gt;echo heartbeat &amp;gt; /sys/class/leds/run-g/trigger&lt;BR /&gt;not&lt;/P&gt;&lt;P&gt;the same is also with&lt;/P&gt;&lt;P&gt;echo 255 &amp;gt; /sys/class/leds/run-g/brightness&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The kernel &lt;A href="https://github.com/Freescale/linux-fslc/tree/5.10-2.1.x-imx" target="_blank"&gt;https://github.com/Freescale/linux-fslc/tree/5.10-2.1.x-imx&lt;/A&gt;&lt;BR /&gt;attached is the device tree and the kernel configuration file&lt;/P&gt;&lt;P&gt;does anyone have any idea, it looks like the LED support for the qoriq gpio drivers is not working?&lt;BR /&gt;Greetings from the island of Rügen&lt;BR /&gt;Jörg Hering&lt;/P&gt;</description>
    <pubDate>Mon, 02 May 2022 06:55:41 GMT</pubDate>
    <dc:creator>jhering_ruegen</dc:creator>
    <dc:date>2022-05-02T06:55:41Z</dc:date>
    <item>
      <title>GPIO LED support LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/GPIO-LED-support-LS1046A/m-p/1451697#M10491</link>
      <description>&lt;P&gt;Hi colleagues,&lt;/P&gt;&lt;P&gt;I am trying to enable LED support via GPIO for our board based on LS1046. In the system I have both mpc8xxx (CONFIG_GPIO_MPC8XXX) based GPIOs and I2C based GPIOs. The LED functionality works for the I2C part e.g.&lt;BR /&gt;echo heartbeat &amp;gt; /sys/class/leds/x1p/trigger&lt;BR /&gt;but for the LS1046 GPIOs&lt;BR /&gt;echo heartbeat &amp;gt; /sys/class/leds/run-g/trigger&lt;BR /&gt;not&lt;/P&gt;&lt;P&gt;the same is also with&lt;/P&gt;&lt;P&gt;echo 255 &amp;gt; /sys/class/leds/run-g/brightness&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The kernel &lt;A href="https://github.com/Freescale/linux-fslc/tree/5.10-2.1.x-imx" target="_blank"&gt;https://github.com/Freescale/linux-fslc/tree/5.10-2.1.x-imx&lt;/A&gt;&lt;BR /&gt;attached is the device tree and the kernel configuration file&lt;/P&gt;&lt;P&gt;does anyone have any idea, it looks like the LED support for the qoriq gpio drivers is not working?&lt;BR /&gt;Greetings from the island of Rügen&lt;BR /&gt;Jörg Hering&lt;/P&gt;</description>
      <pubDate>Mon, 02 May 2022 06:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/GPIO-LED-support-LS1046A/m-p/1451697#M10491</guid>
      <dc:creator>jhering_ruegen</dc:creator>
      <dc:date>2022-05-02T06:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO LED support LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/GPIO-LED-support-LS1046A/m-p/1467972#M10616</link>
      <description>&lt;P&gt;Please refer to the following document to verify GPIO in sysfs.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/LS1043-GPIO-support-in-Linux-SDK/ta-p/1103689" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/LS1043-GPIO-support-in-Linux-SDK/ta-p/1103689&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jun 2022 05:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/GPIO-LED-support-LS1046A/m-p/1467972#M10616</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-02T05:34:55Z</dc:date>
    </item>
  </channel>
</rss>