<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 [LS1046] RGMII initialization</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-RGMII-initialization/m-p/1448179#M10436</link>
    <description>&lt;P&gt;I'm trying to run uboot in my ls1046 board. this board is developed by our colleagues. now, SGMII can work. but MAC3/MAC4 RGMII cannot work normally(seems link OK, but ping/tftp failed).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PHY device is&amp;nbsp;RX8010 which mode select by hardware pins.&lt;/P&gt;&lt;P&gt;I checked the RCW[EC1] /&amp;nbsp;RCW[EC2] /RCW[EM1] / RCW[EM2] and the SCFT_ECGTXCMCR configuration. Any other issue that I missed?&lt;/P&gt;&lt;P&gt;following cited from uboot console&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt; tftpboot 82000000 u-boot.bin&lt;BR /&gt;genphy_update_link mii_reg=7949&lt;BR /&gt;drivers/net/phy/phy.c fm1-mac2 Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;BR /&gt;fm1-mac2: Could not initialize&lt;BR /&gt;genphy_update_link mii_reg=7949&lt;BR /&gt;drivers/net/phy/phy.c fm1-mac3 Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;BR /&gt;fm1-mac3: Could not initialize&lt;BR /&gt;genphy_update_link mii_reg=796d&lt;BR /&gt;genphy_parse_link mii_reg=796d&lt;BR /&gt;Using fm1-mac4 device&lt;BR /&gt;TFTP from server 192.168.10.101; our IP address is 192.168.10.100&lt;BR /&gt;Filename 'u-boot.bin'.&lt;BR /&gt;Load address: 0x82000000&lt;BR /&gt;Loading: *&lt;BR /&gt;ARP Retry count exceeded; starting again&lt;BR /&gt;=&amp;gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 24 Apr 2022 09:16:43 GMT</pubDate>
    <dc:creator>linxx</dc:creator>
    <dc:date>2022-04-24T09:16:43Z</dc:date>
    <item>
      <title>[LS1046] RGMII initialization</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-RGMII-initialization/m-p/1448179#M10436</link>
      <description>&lt;P&gt;I'm trying to run uboot in my ls1046 board. this board is developed by our colleagues. now, SGMII can work. but MAC3/MAC4 RGMII cannot work normally(seems link OK, but ping/tftp failed).&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PHY device is&amp;nbsp;RX8010 which mode select by hardware pins.&lt;/P&gt;&lt;P&gt;I checked the RCW[EC1] /&amp;nbsp;RCW[EC2] /RCW[EM1] / RCW[EM2] and the SCFT_ECGTXCMCR configuration. Any other issue that I missed?&lt;/P&gt;&lt;P&gt;following cited from uboot console&amp;nbsp;&lt;/P&gt;&lt;P&gt;=&amp;gt; tftpboot 82000000 u-boot.bin&lt;BR /&gt;genphy_update_link mii_reg=7949&lt;BR /&gt;drivers/net/phy/phy.c fm1-mac2 Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;BR /&gt;fm1-mac2: Could not initialize&lt;BR /&gt;genphy_update_link mii_reg=7949&lt;BR /&gt;drivers/net/phy/phy.c fm1-mac3 Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;BR /&gt;fm1-mac3: Could not initialize&lt;BR /&gt;genphy_update_link mii_reg=796d&lt;BR /&gt;genphy_parse_link mii_reg=796d&lt;BR /&gt;Using fm1-mac4 device&lt;BR /&gt;TFTP from server 192.168.10.101; our IP address is 192.168.10.100&lt;BR /&gt;Filename 'u-boot.bin'.&lt;BR /&gt;Load address: 0x82000000&lt;BR /&gt;Loading: *&lt;BR /&gt;ARP Retry count exceeded; starting again&lt;BR /&gt;=&amp;gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 24 Apr 2022 09:16:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-RGMII-initialization/m-p/1448179#M10436</guid>
      <dc:creator>linxx</dc:creator>
      <dc:date>2022-04-24T09:16:43Z</dc:date>
    </item>
  </channel>
</rss>