<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1043A Board Bring up in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-Board-Bring-up/m-p/1443948#M10383</link>
    <description>&lt;P&gt;You need to use CodeWarrior +CodeWarrior TAP/CMSIS DAP to connect to the target board to program firmware.&lt;/P&gt;
&lt;P&gt;You also could prepare SD card bootloader and write firmware to SD card with "dd" command in Linux.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Apr 2022 08:12:01 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-04-14T08:12:01Z</dc:date>
    <item>
      <title>LS1043A Board Bring up</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Board-Bring-up/m-p/1441431#M10360</link>
      <description>&lt;P&gt;I was asked by management if the only way to bring up an LS1043A board was using a JTAG and Code Warrior.&amp;nbsp; Is there any other method of board bring up?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know the i.MX series has IMX_USB for serial downloads, but I can not find a similar method for the LS1043A.&lt;/P&gt;&lt;P&gt;Page 35 of this document (&amp;nbsp;AMF-NET-T2776.pdf ) indicates that the JTAG and CW are needed to load the u-boot image and from that point we can use tftp to load the Linux Kernel and other files.&amp;nbsp;&lt;/P&gt;&lt;P&gt;TIA.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Apr 2022 16:37:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Board-Bring-up/m-p/1441431#M10360</guid>
      <dc:creator>gfine1</dc:creator>
      <dc:date>2022-04-08T16:37:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A Board Bring up</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Board-Bring-up/m-p/1443948#M10383</link>
      <description>&lt;P&gt;You need to use CodeWarrior +CodeWarrior TAP/CMSIS DAP to connect to the target board to program firmware.&lt;/P&gt;
&lt;P&gt;You also could prepare SD card bootloader and write firmware to SD card with "dd" command in Linux.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Apr 2022 08:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Board-Bring-up/m-p/1443948#M10383</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-04-14T08:12:01Z</dc:date>
    </item>
  </channel>
</rss>