<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 LS1021 DCU resolution</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381017#M103</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are evaluating HDMI port on TWR-LS1021A board where trying to change video resolution dynamically or at least set higher one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have successfully build fsl-image-x11 image and boot it on the target board (SDK 1.3)&lt;/P&gt;&lt;P&gt;u-boot: enabling video mode works as expected (640x480)&lt;/P&gt;&lt;P&gt;linux: X11 output works using smallest resolution offered by monitor (720x400)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is correct way to change resolution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Avaliable modes from monitor:&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# cat /sys/class/graphics/fb0/modes &lt;/P&gt;&lt;P&gt;S:1280x960p-60&lt;/P&gt;&lt;P&gt;V:1024x768p-60&lt;/P&gt;&lt;P&gt;V:800x600p-60&lt;/P&gt;&lt;P&gt;V:640x480p-60&lt;/P&gt;&lt;P&gt;U:720x400p-70&lt;/P&gt;&lt;P&gt;D:1280x1024p-60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;xrand info:&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr &lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;Screen 0: minimum 720 x 400, current 720 x 400, maximum 720 x 400&lt;/P&gt;&lt;P&gt;default connected 720x400+0+0 0mm x 0mm&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 720x400&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 70.0* &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;xrandr, adding new mode and applying with xrand:&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# cvt 640 480 60 -v&lt;/P&gt;&lt;P&gt;# 640x480 59.38 Hz (CVT 0.31M3) hsync: 29.69 kHz; pclk: 23.75 MHz&lt;/P&gt;&lt;P&gt;Modeline "640x480_60.00"&amp;nbsp;&amp;nbsp; 23.75&amp;nbsp; 640 664 720 800&amp;nbsp; 480 483 487 500 -hsync +vsync&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --newmode "640x480_60.00" 23.75&amp;nbsp; 640 664 720 800&amp;nbsp; 480 483 487 500 -hsync +vsync&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --addmode default 640x480_60.00&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --output default --mode 640x480_60.00&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;xrandr: screen cannot be larger than 720x400 (desired size 640x480)&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --output default --mode 640x480_60.00&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;xrandr: Configure crtc 0 failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also other resolutions were tested. First setting fb mode directly (/sys/class/graphics/fb0/mode) does not help either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any hints?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, Klemen&lt;/P&gt;&lt;DIV class="column"&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Dec 2014 14:15:29 GMT</pubDate>
    <dc:creator>kporenta</dc:creator>
    <dc:date>2014-12-30T14:15:29Z</dc:date>
    <item>
      <title>LS1021 DCU resolution</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381017#M103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we are evaluating HDMI port on TWR-LS1021A board where trying to change video resolution dynamically or at least set higher one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have successfully build fsl-image-x11 image and boot it on the target board (SDK 1.3)&lt;/P&gt;&lt;P&gt;u-boot: enabling video mode works as expected (640x480)&lt;/P&gt;&lt;P&gt;linux: X11 output works using smallest resolution offered by monitor (720x400)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is correct way to change resolution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Avaliable modes from monitor:&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# cat /sys/class/graphics/fb0/modes &lt;/P&gt;&lt;P&gt;S:1280x960p-60&lt;/P&gt;&lt;P&gt;V:1024x768p-60&lt;/P&gt;&lt;P&gt;V:800x600p-60&lt;/P&gt;&lt;P&gt;V:640x480p-60&lt;/P&gt;&lt;P&gt;U:720x400p-70&lt;/P&gt;&lt;P&gt;D:1280x1024p-60&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;xrand info:&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr &lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;Screen 0: minimum 720 x 400, current 720 x 400, maximum 720 x 400&lt;/P&gt;&lt;P&gt;default connected 720x400+0+0 0mm x 0mm&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; 720x400&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 70.0* &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;xrandr, adding new mode and applying with xrand:&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# cvt 640 480 60 -v&lt;/P&gt;&lt;P&gt;# 640x480 59.38 Hz (CVT 0.31M3) hsync: 29.69 kHz; pclk: 23.75 MHz&lt;/P&gt;&lt;P&gt;Modeline "640x480_60.00"&amp;nbsp;&amp;nbsp; 23.75&amp;nbsp; 640 664 720 800&amp;nbsp; 480 483 487 500 -hsync +vsync&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --newmode "640x480_60.00" 23.75&amp;nbsp; 640 664 720 800&amp;nbsp; 480 483 487 500 -hsync +vsync&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --addmode default 640x480_60.00&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --output default --mode 640x480_60.00&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;xrandr: screen cannot be larger than 720x400 (desired size 640x480)&lt;/P&gt;&lt;P&gt;root@ls1021atwr:~# xrandr --output default --mode 640x480_60.00&lt;/P&gt;&lt;P&gt;xrandr: Failed to get size of gamma for output default&lt;/P&gt;&lt;P&gt;xrandr: Configure crtc 0 failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also other resolutions were tested. First setting fb mode directly (/sys/class/graphics/fb0/mode) does not help either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any hints?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you, Klemen&lt;/P&gt;&lt;DIV class="column"&gt;&lt;P&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Dec 2014 14:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381017#M103</guid>
      <dc:creator>kporenta</dc:creator>
      <dc:date>2014-12-30T14:15:29Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021 DCU resolution</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381018#M104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Adding new modes to xorg.conf does the trick.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/usr/share/X11/xorg.conf.d/10-monitor.conf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section "Monitor"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Identifier "Monitor0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Modeline "640x480_60.00"&amp;nbsp;&amp;nbsp; 23.75&amp;nbsp; 640 664 720 800&amp;nbsp; 480 483 487 500 -hsync +vsync&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Modeline "800x600_60.00"&amp;nbsp;&amp;nbsp; 38.25&amp;nbsp; 800 832 912 1024&amp;nbsp; 600 603 607 624 -hsync +vsync&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Modeline "1024x768_60.00"&amp;nbsp;&amp;nbsp; 63.50&amp;nbsp; 1024 1072 1176 1328&amp;nbsp; 768 771 775 798 -hsync +vsync&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Modeline "1280x1024_60.00"&amp;nbsp; 109.00&amp;nbsp; 1280 1368 1496 1712&amp;nbsp; 1024 1027 1034 1063 -hsync +vsync&lt;/P&gt;&lt;P&gt;EndSection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section "Device"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Identifier "Device0"&lt;/P&gt;&lt;P&gt;EndSection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Section "Screen"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Identifier "Screen0" &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Device "Device0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Monitor "Monitor0"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DefaultDepth 16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SubSection "Display"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Depth 16&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Modes "640x480_60.00"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; EndSubSection&lt;/P&gt;&lt;P&gt;EndSection&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;... but only for 640x480. Using any other mode, Xserver crashes, Segmentation fault&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;[2632130.375] (II) FBDEV(0): using default device&lt;/P&gt;&lt;P&gt;[2632130.381] (**) FBDEV(0): Depth 16, (--) framebuffer bpp 16&lt;/P&gt;&lt;P&gt;[2632130.381] (==) FBDEV(0): RGB weight 565&lt;/P&gt;&lt;P&gt;[2632130.381] (==) FBDEV(0): Default visual is TrueColor&lt;/P&gt;&lt;P&gt;[2632130.381] (==) FBDEV(0): Using gamma correction (1.0, 1.0, 1.0)&lt;/P&gt;&lt;P&gt;[2632130.381] (II) FBDEV(0): hardware:&amp;nbsp; (video memory: 843kB)&lt;/P&gt;&lt;P&gt;[2632130.381] (II) FBDEV(0): checking modes against framebuffer device...&lt;/P&gt;&lt;P&gt;[2632130.381] (II) FBDEV(0):&amp;nbsp;&amp;nbsp;&amp;nbsp; mode "800x600_60.00" ok&lt;/P&gt;&lt;P&gt;[2632130.381] (II) FBDEV(0): checking modes against monitor...&lt;/P&gt;&lt;P&gt;[2632130.381] (--) FBDEV(0): Virtual size is 800x600 (pitch 800)&lt;/P&gt;&lt;P&gt;[2632130.381] (**) FBDEV(0):&amp;nbsp; Mode "800x600_60.00": 38.2 MHz (scaled from 0.0 MHz), 37.4 kHz, 59.9 Hz&lt;/P&gt;&lt;P&gt;[2632130.381] (II) FBDEV(0): Modeline "800x600_60.00"x0.0&amp;nbsp;&amp;nbsp; 38.25&amp;nbsp; 800 832 912 1024&amp;nbsp; 600 603 607 624 -hsync +vsync (37.4 kHz)&lt;/P&gt;&lt;P&gt;[2632130.381] (==) FBDEV(0): DPI set to (96, 96)&lt;/P&gt;&lt;P&gt;[2632130.381] (II) Loading sub module "fb"&lt;/P&gt;&lt;P&gt;[2632130.381] (II) LoadModule: "fb"&lt;/P&gt;&lt;P&gt;[2632130.382] (II) Loading /usr/lib/xorg/modules/libfb.so&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;[2632130.937] (EE) &lt;/P&gt;&lt;P&gt;[2632130.938] (EE) Backtrace:&lt;/P&gt;&lt;P&gt;[2632130.938] (EE) &lt;/P&gt;&lt;P&gt;[2632130.938] (EE) Segmentation fault at address 0x76a42000&lt;/P&gt;&lt;P&gt;[2632130.938] &lt;/P&gt;&lt;P&gt;Fatal server error:&lt;/P&gt;&lt;P&gt;[2632130.938] Caught signal 11 (Segmentation fault). Server aborting&lt;/P&gt;&lt;P&gt;[2632130.938] &lt;/P&gt;&lt;P&gt;[2632130.938] (EE) &lt;/P&gt;&lt;P&gt;.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br, Klemen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Dec 2014 22:16:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381018#M104</guid>
      <dc:creator>kporenta</dc:creator>
      <dc:date>2014-12-30T22:16:39Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021 DCU resolution</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381019#M105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Setting FB DCU buffer to higher value solves segmentation fault. This is done by setting bootarg "res=" to desired value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No need for &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;xorg.conf&lt;/SPAN&gt; if bootarg is set.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Jan 2015 19:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021-DCU-resolution/m-p/381019#M105</guid>
      <dc:creator>kporenta</dc:creator>
      <dc:date>2015-01-03T19:20:11Z</dc:date>
    </item>
  </channel>
</rss>