<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Packrfs failed? ubuntu is incomplete in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432360#M10267</link>
    <description>&lt;P&gt;The packrfs command is supposed to generate rootfs, but when this error is printed, rootfs was not generated in the image folder.&amp;nbsp;In other words, packrfs has failed.&lt;/P&gt;&lt;P&gt;However, as shown above, it only shows "incomplete", so it is unclear why it is failing. What is the cause of the error?&lt;/P&gt;</description>
    <pubDate>Wed, 23 Mar 2022 04:50:26 GMT</pubDate>
    <dc:creator>m_kei</dc:creator>
    <dc:date>2022-03-23T04:50:26Z</dc:date>
    <item>
      <title>Packrfs failed? ubuntu is incomplete</title>
      <link>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432359#M10266</link>
      <description>&lt;P&gt;I am trying to generate RFS in LSDK2108.&amp;nbsp;We are trying to build userland by referring to "How to build various userland with custom packages" in the LSDK2108 user guide.&lt;/P&gt;&lt;P&gt;Whenever I run "flex-builder -i packrfs", I get something like the following error message.&lt;/P&gt;&lt;P&gt;/xxx/flexbuild_lsdk2108/build/rfs/rootfs_lsdk2108_ubuntu_main_arm64 is incomplete&lt;/P&gt;&lt;P&gt;Since no further messages are output, it is difficult to tell if this is an error or not. What kind of output message is this?&lt;/P&gt;&lt;P&gt;Is it an error? Or is it an advice to continue doing mkboot?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 04:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432359#M10266</guid>
      <dc:creator>m_kei</dc:creator>
      <dc:date>2022-03-23T04:43:40Z</dc:date>
    </item>
    <item>
      <title>Re: Packrfs failed? ubuntu is incomplete</title>
      <link>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432360#M10267</link>
      <description>&lt;P&gt;The packrfs command is supposed to generate rootfs, but when this error is printed, rootfs was not generated in the image folder.&amp;nbsp;In other words, packrfs has failed.&lt;/P&gt;&lt;P&gt;However, as shown above, it only shows "incomplete", so it is unclear why it is failing. What is the cause of the error?&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 04:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432360#M10267</guid>
      <dc:creator>m_kei</dc:creator>
      <dc:date>2022-03-23T04:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: Packrfs failed? ubuntu is incomplete</title>
      <link>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432364#M10268</link>
      <description>&lt;P&gt;The cause seems to have been a corrupted file in build/rfs or some other problem.&lt;/P&gt;&lt;P&gt;For some reason, build/rfs was not erased even with cleanrfs, and because of the corrupted rfs file, the rootfs is not created in mkrfs, resulting in an error that there is no target rootfs as packrfs.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Mar 2022 04:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1432364#M10268</guid>
      <dc:creator>m_kei</dc:creator>
      <dc:date>2022-03-23T04:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: Packrfs failed? ubuntu is incomplete</title>
      <link>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1721204#M13274</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;which is the cause and the solution for this kind of error?&lt;/P&gt;</description>
      <pubDate>Tue, 12 Sep 2023 12:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Packrfs-failed-ubuntu-is-incomplete/m-p/1721204#M13274</guid>
      <dc:creator>mdecandia</dc:creator>
      <dc:date>2023-09-12T12:11:56Z</dc:date>
    </item>
  </channel>
</rss>