<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to edit .scr boot script file to boot Linux from uboot in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-to-edit-scr-boot-script-file-to-boot-Linux-from-uboot/m-p/1425699#M10192</link>
    <description>&lt;P&gt;In LSDK, a script file named *.scr is used to boot Linux on the SD card from uboot.&lt;BR /&gt;How do I edit this *.scr file, more specifically lx2160ardb_boot.scr?&lt;/P&gt;&lt;P&gt;As far as searching in the build folder, there are .scr files for various boards in the uboot folder.&amp;nbsp;I think "flex-builder -i mkimage" only selects and copies the .scr file from the board specified by the "-m" option from the .scr file that exists in the uboot folder.&lt;/P&gt;&lt;P&gt;So I assume that somewhere during the "flex-builder -i atf" run that generates the uboot, a .scr file is generated, where is this done?&amp;nbsp;Also, is it possible to generate a .scr file with different contents?&lt;/P&gt;</description>
    <pubDate>Thu, 10 Mar 2022 01:39:33 GMT</pubDate>
    <dc:creator>m_kei</dc:creator>
    <dc:date>2022-03-10T01:39:33Z</dc:date>
    <item>
      <title>How to edit .scr boot script file to boot Linux from uboot</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-edit-scr-boot-script-file-to-boot-Linux-from-uboot/m-p/1425699#M10192</link>
      <description>&lt;P&gt;In LSDK, a script file named *.scr is used to boot Linux on the SD card from uboot.&lt;BR /&gt;How do I edit this *.scr file, more specifically lx2160ardb_boot.scr?&lt;/P&gt;&lt;P&gt;As far as searching in the build folder, there are .scr files for various boards in the uboot folder.&amp;nbsp;I think "flex-builder -i mkimage" only selects and copies the .scr file from the board specified by the "-m" option from the .scr file that exists in the uboot folder.&lt;/P&gt;&lt;P&gt;So I assume that somewhere during the "flex-builder -i atf" run that generates the uboot, a .scr file is generated, where is this done?&amp;nbsp;Also, is it possible to generate a .scr file with different contents?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 01:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-edit-scr-boot-script-file-to-boot-Linux-from-uboot/m-p/1425699#M10192</guid>
      <dc:creator>m_kei</dc:creator>
      <dc:date>2022-03-10T01:39:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to edit .scr boot script file to boot Linux from uboot</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-edit-scr-boot-script-file-to-boot-Linux-from-uboot/m-p/1426714#M10208</link>
      <description>&lt;P&gt;You could modify section&amp;nbsp;[distro autoboot script] in&amp;nbsp;configs/board/lx2160ardb_rev2/manifest&lt;/P&gt;
&lt;P&gt;Then regenerate boot script with the following command.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;$ flex-builder -i mkdistroscr -m&amp;nbsp;lx2160ardb_rev2&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 07:58:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-edit-scr-boot-script-file-to-boot-Linux-from-uboot/m-p/1426714#M10208</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-03-11T07:58:54Z</dc:date>
    </item>
  </channel>
</rss>