<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic qbvset, qbvget doesn't work on LS1028ardb in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1417598#M10106</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm using LS1028ARDB and I tested tsntool on LS1028ardb.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I didn't build or configure linux, I just installed LSDK 21.08 using flex-installer.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I connected two NVIDIA jetson agx xavier boards to the swp0, swp1 port to test tsn on LS1028ardb. (xavier 1-swp0 , xavier 2-swp1) And&amp;nbsp;xavier 1 send packets to xavier 2.&lt;/P&gt;&lt;P&gt;I configured switch through the command below.&lt;/P&gt;&lt;P&gt;INTERFACES="swp0 swp1 swp2 swp3"&lt;/P&gt;&lt;P&gt;ip link set eno2 up&lt;BR /&gt;ip link add name br0 type bridge&lt;BR /&gt;for if in $INTERFACES;&lt;BR /&gt;do&lt;BR /&gt;ip link set dev $if master br0&lt;BR /&gt;ip link set $if up&lt;BR /&gt;done&lt;BR /&gt;ip link set br0 up&lt;/P&gt;&lt;P&gt;bridge link show&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5: swp0@eno2: &amp;lt;BROADCAST,MULTICAST,UP,LOWER_UP&amp;gt; mtu 1500 master br0 state forwarding priority 32 cost 4&lt;BR /&gt;6: swp1@eno2: &amp;lt;BROADCAST,MULTICAST,UP,LOWER_UP&amp;gt; mtu 1500 master br0 state forwarding priority 32 cost 4&lt;BR /&gt;7: swp2@eno2: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 master br0 state disabled priority 32 cost 100&lt;BR /&gt;8: swp3@eno2: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 master br0 state disabled priority 32 cost 100&lt;BR /&gt;10: virbr0-nic: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1500 master virbr0 state disabled priority 32 cost 100&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I tested qbvset using tsntool command referring to&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-DFCCABAD-ABA2-4F8C-A91D-73C1B1357670.html" target="_self"&gt;qbv test&lt;/A&gt;&amp;nbsp;. But it doesn't work.&lt;/P&gt;&lt;P&gt;tsntool&amp;gt; qbvset --device swp1 --entryfile qbv0.txt&lt;/P&gt;&lt;P&gt;echo reply:swp1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo reply:-19&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The same goes for qbvget.&lt;/P&gt;&lt;P&gt;tsntool&amp;gt; qbvget --device swp1&lt;/P&gt;&lt;P&gt;echo reply:swp1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo reply:-19&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it works to 'eno2' port. If I set the address 192.168.1.2 in br0 interface and ping 192.168.1.2 in xavier 1, the packet is not sent. (qbv0.txt "t0 00000000b 20000")&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Why doesn't qbvset and qbvget work on the swpX&lt;/STRONG&gt; &lt;STRONG&gt;port?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is this a problem with tsntool? Or is it because the kernel was not built by setting up the TSN-related configuration?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Feb 2022 16:00:07 GMT</pubDate>
    <dc:creator>JE-KIM</dc:creator>
    <dc:date>2022-02-22T16:00:07Z</dc:date>
    <item>
      <title>qbvset, qbvget doesn't work on LS1028ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1417598#M10106</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm using LS1028ARDB and I tested tsntool on LS1028ardb.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I didn't build or configure linux, I just installed LSDK 21.08 using flex-installer.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I connected two NVIDIA jetson agx xavier boards to the swp0, swp1 port to test tsn on LS1028ardb. (xavier 1-swp0 , xavier 2-swp1) And&amp;nbsp;xavier 1 send packets to xavier 2.&lt;/P&gt;&lt;P&gt;I configured switch through the command below.&lt;/P&gt;&lt;P&gt;INTERFACES="swp0 swp1 swp2 swp3"&lt;/P&gt;&lt;P&gt;ip link set eno2 up&lt;BR /&gt;ip link add name br0 type bridge&lt;BR /&gt;for if in $INTERFACES;&lt;BR /&gt;do&lt;BR /&gt;ip link set dev $if master br0&lt;BR /&gt;ip link set $if up&lt;BR /&gt;done&lt;BR /&gt;ip link set br0 up&lt;/P&gt;&lt;P&gt;bridge link show&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;5: swp0@eno2: &amp;lt;BROADCAST,MULTICAST,UP,LOWER_UP&amp;gt; mtu 1500 master br0 state forwarding priority 32 cost 4&lt;BR /&gt;6: swp1@eno2: &amp;lt;BROADCAST,MULTICAST,UP,LOWER_UP&amp;gt; mtu 1500 master br0 state forwarding priority 32 cost 4&lt;BR /&gt;7: swp2@eno2: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 master br0 state disabled priority 32 cost 100&lt;BR /&gt;8: swp3@eno2: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 master br0 state disabled priority 32 cost 100&lt;BR /&gt;10: virbr0-nic: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1500 master virbr0 state disabled priority 32 cost 100&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I tested qbvset using tsntool command referring to&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-DFCCABAD-ABA2-4F8C-A91D-73C1B1357670.html" target="_self"&gt;qbv test&lt;/A&gt;&amp;nbsp;. But it doesn't work.&lt;/P&gt;&lt;P&gt;tsntool&amp;gt; qbvset --device swp1 --entryfile qbv0.txt&lt;/P&gt;&lt;P&gt;echo reply:swp1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo reply:-19&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The same goes for qbvget.&lt;/P&gt;&lt;P&gt;tsntool&amp;gt; qbvget --device swp1&lt;/P&gt;&lt;P&gt;echo reply:swp1&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;echo reply:-19&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it works to 'eno2' port. If I set the address 192.168.1.2 in br0 interface and ping 192.168.1.2 in xavier 1, the packet is not sent. (qbv0.txt "t0 00000000b 20000")&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Why doesn't qbvset and qbvget work on the swpX&lt;/STRONG&gt; &lt;STRONG&gt;port?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Is this a problem with tsntool? Or is it because the kernel was not built by setting up the TSN-related configuration?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 16:00:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1417598#M10106</guid>
      <dc:creator>JE-KIM</dc:creator>
      <dc:date>2022-02-22T16:00:07Z</dc:date>
    </item>
    <item>
      <title>Re: qbvset, qbvget doesn't work on LS1028ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1418135#M10113</link>
      <description>&lt;P&gt;You need to enable "MSCC_FELIX_SWITCH_TSN" in Linux Kernel configuration file, which is not enabled by default.&lt;/P&gt;
&lt;P&gt;You could refer to section "8.8.1.2 Kernel configuration" in LSDK 21.08 user guide.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Feb 2022 09:51:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1418135#M10113</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-02-23T09:51:18Z</dc:date>
    </item>
    <item>
      <title>Re: qbvset, qbvget doesn't work on LS1028ardb</title>
      <link>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1421845#M10157</link>
      <description>&lt;P&gt;I built linux kernel (4.19) using flex-builder and config file and qbvset, qbvget worked for swpX ports. (&lt;SPAN&gt;I attached the used config file.)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;However, although the switch configuration was performed by referring to&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-6CEF5D8C-2681-4206-9236-034442711422.html" target="_self"&gt;Switch Configuration&lt;/A&gt;&amp;nbsp;, packets between the boards(connected to swp0, swp1) are not transmitted.&lt;/P&gt;&lt;P&gt;When checked with the $ ip link show as below, it seems that there is no connection between the swpX ports and eno2 port unlike&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-CBD176F9-EE56-4A30-8E93-BB0D4F480793.html" target="_self"&gt;Felix interfaces&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;$ ip link show&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;1: lo: &amp;lt;LOOPBACK,UP,LOWER_UP&amp;gt; mtu 65536 qdisc noqueue state UNKNOWN mode DEFAULT group default qlen 1&lt;BR /&gt;000&lt;BR /&gt;link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00&lt;BR /&gt;2: eno0: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether 22:79:ea:65:b1:bd brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;3: eno2: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1500 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether ba:ec:d4:e0:c3:22 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;4: swp0: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1468 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether aa:bc:77:9d:eb:a0 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;5: swp1: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1468 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether aa:bc:77:9d:eb:a1 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;6: swp2: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1468 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether aa:bc:77:9d:eb:a2 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;7: swp3: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1468 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether aa:bc:77:9d:eb:a3 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;8: swp4: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1468 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/ether aa:bc:77:9d:eb:a4 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;9: sit0@NONE: &amp;lt;NOARP&amp;gt; mtu 1480 qdisc noop state DOWN mode DEFAULT group default qlen 1000&lt;BR /&gt;link/sit 0.0.0.0 brd 0.0.0.0&lt;BR /&gt;10: virbr0: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 qdisc noqueue state DOWN mode DEFAULT group&lt;BR /&gt;default qlen 1000&lt;BR /&gt;link/ether 52:54:00:44:42:04 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;11: virbr0-nic: &amp;lt;BROADCAST,MULTICAST&amp;gt; mtu 1500 qdisc pfifo_fast master virbr0 state DOWN mode DEFAULT&lt;BR /&gt;group default qlen 1000&lt;BR /&gt;link/ether 52:54:00:44:42:04 brd ff:ff:ff:ff:ff:ff&lt;BR /&gt;12: docker0: &amp;lt;NO-CARRIER,BROADCAST,MULTICAST,UP&amp;gt; mtu 1500 qdisc noqueue state DOWN mode DEFAULT group&lt;BR /&gt;default&lt;BR /&gt;link/ether 02:42:ec:cf:65:08 brd ff:ff:ff:ff:ff:ff&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@localhost:~# &lt;STRONG&gt;brctl show&lt;/STRONG&gt;&lt;BR /&gt;bridge name&amp;nbsp; bridge id&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;STP enabled&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;interfaces&lt;BR /&gt;br0&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;8000.aabc779deba0&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;no&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; swp0&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; swp1&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; swp2&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; swp3&lt;BR /&gt;docker0&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;8000.0242eccf6508&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;no&lt;BR /&gt;virbr0&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;8000.525400444204&amp;nbsp; &amp;nbsp; &amp;nbsp; yes&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; virbr0-nic&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is the kernel build wrong?...&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Mar 2022 10:49:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/qbvset-qbvget-doesn-t-work-on-LS1028ardb/m-p/1421845#M10157</guid>
      <dc:creator>JE-KIM</dc:creator>
      <dc:date>2022-03-02T10:49:44Z</dc:date>
    </item>
  </channel>
</rss>