<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLA1028A EEPROM problem consultation</title>
    <link>https://community.nxp.com/t5/Layerscape/LA1028A-EEPROM-problem-consultation/m-p/1416295#M10087</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;In the LS1028A schematic, there are three different EEPROM devices, what are the functions respectively?&lt;/SPAN&gt;&lt;SPAN class=""&gt; Is there a detailed documentation?&lt;/SPAN&gt;&lt;SPAN class=""&gt; In the design, can it be removed?&lt;/SPAN&gt;&lt;SPAN class=""&gt; Thank you very much!&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="微信图片_20220220122001.png" style="width: 872px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171109i2615E6E3358628A5/image-size/large?v=v2&amp;amp;px=999" role="button" title="微信图片_20220220122001.png" alt="微信图片_20220220122001.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Sun, 20 Feb 2022 04:41:19 GMT</pubDate>
    <dc:creator>jack_huang1</dc:creator>
    <dc:date>2022-02-20T04:41:19Z</dc:date>
    <item>
      <title>LA1028A EEPROM problem consultation</title>
      <link>https://community.nxp.com/t5/Layerscape/LA1028A-EEPROM-problem-consultation/m-p/1416295#M10087</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;In the LS1028A schematic, there are three different EEPROM devices, what are the functions respectively?&lt;/SPAN&gt;&lt;SPAN class=""&gt; Is there a detailed documentation?&lt;/SPAN&gt;&lt;SPAN class=""&gt; In the design, can it be removed?&lt;/SPAN&gt;&lt;SPAN class=""&gt; Thank you very much!&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="微信图片_20220220122001.png" style="width: 872px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171109i2615E6E3358628A5/image-size/large?v=v2&amp;amp;px=999" role="button" title="微信图片_20220220122001.png" alt="微信图片_20220220122001.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Feb 2022 04:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LA1028A-EEPROM-problem-consultation/m-p/1416295#M10087</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2022-02-20T04:41:19Z</dc:date>
    </item>
    <item>
      <title>Re: LA1028A EEPROM problem consultation</title>
      <link>https://community.nxp.com/t5/Layerscape/LA1028A-EEPROM-problem-consultation/m-p/1416300#M10088</link>
      <description>&lt;P&gt;Please refer to the QorIQ LS1028A Reference Design Board Reference Manual, Table 15. I2C1 bus device map.&lt;/P&gt;
&lt;P&gt;&amp;gt; &lt;SPAN class=""&gt;In the design, can it be removed?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;U47 can be removed if booting from I2C is not needed.&lt;/P&gt;
&lt;P&gt;U50 can be removed if hard-coded DDR controller settings are provided in the TF-A BL2.&lt;/P&gt;</description>
      <pubDate>Sun, 20 Feb 2022 06:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LA1028A-EEPROM-problem-consultation/m-p/1416300#M10088</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-02-20T06:12:01Z</dc:date>
    </item>
  </channel>
</rss>