<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Load (for booting) the bl2.pbl and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Load-for-booting-the-bl2-pbl-and-fip-bin-file-via-CodeWarrior/m-p/1413408#M10040</link>
    <description>&lt;P&gt;How do I load (for booting) the bl2.pbl (RCW+PBI+BL2) and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?&lt;/P&gt;&lt;P&gt;Do I need to make any changes in the source code (rcw, pbl and uboot) to support the loading via JTAG?&lt;/P&gt;</description>
    <pubDate>Tue, 15 Feb 2022 04:22:42 GMT</pubDate>
    <dc:creator>ts1234</dc:creator>
    <dc:date>2022-02-15T04:22:42Z</dc:date>
    <item>
      <title>Load (for booting) the bl2.pbl and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/Load-for-booting-the-bl2-pbl-and-fip-bin-file-via-CodeWarrior/m-p/1413408#M10040</link>
      <description>&lt;P&gt;How do I load (for booting) the bl2.pbl (RCW+PBI+BL2) and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?&lt;/P&gt;&lt;P&gt;Do I need to make any changes in the source code (rcw, pbl and uboot) to support the loading via JTAG?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Feb 2022 04:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Load-for-booting-the-bl2-pbl-and-fip-bin-file-via-CodeWarrior/m-p/1413408#M10040</guid>
      <dc:creator>ts1234</dc:creator>
      <dc:date>2022-02-15T04:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: Load (for booting) the bl2.pbl and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/Load-for-booting-the-bl2-pbl-and-fip-bin-file-via-CodeWarrior/m-p/1415193#M10070</link>
      <description>&lt;P&gt;After installing CodeWarrior, please refer to section "7.7 Using flash programmer from eclipse IDE" in&amp;nbsp;C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to do flash programming with CodeWarrior IDE.&lt;/P&gt;
&lt;P&gt;Please program&amp;nbsp;&lt;SPAN&gt;bl2.pbl&amp;nbsp; at&amp;nbsp;0x60000000 and&amp;nbsp;fip.bin at&amp;nbsp;0x60100000.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You could refer to section 1 in&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872?attachment-id=18546" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-boot-and-Linux-Kernel-and/ta-p/1114872?attachment-id=18546&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Feb 2022 09:42:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Load-for-booting-the-bl2-pbl-and-fip-bin-file-via-CodeWarrior/m-p/1415193#M10070</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-02-17T09:42:29Z</dc:date>
    </item>
  </channel>
</rss>