<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1088 Throughput test setup</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1088-Throughput-test-setup/m-p/1412953#M10034</link>
    <description>&lt;P&gt;&lt;SPAN&gt;The numbers specified in the DPAA2 Low-level hardware reference manual are the maximum values for the&amp;nbsp; WRIOP engine version present in&amp;nbsp; LS1088.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 14 Feb 2022 08:12:14 GMT</pubDate>
    <dc:creator>andrei_skok</dc:creator>
    <dc:date>2022-02-14T08:12:14Z</dc:date>
    <item>
      <title>LS1088 Throughput test setup</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088-Throughput-test-setup/m-p/1408709#M9989</link>
      <description>&lt;P&gt;In the DPAA2 Low-level hardware reference manual section 7.3.1, the LS1088A is specified as supporting 30Mpps through its two 10G ports with 64B packets. What is the test setup necessary to achieve this? I am unable to achieve more than around 2Mpps. Does the DPAA2 need to be configured in a specific way? Are there patches which must be applied to Linux? Are you using the kernel networking stack or DPDK?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Feb 2022 17:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088-Throughput-test-setup/m-p/1408709#M9989</guid>
      <dc:creator>stadium_aquino</dc:creator>
      <dc:date>2022-02-03T17:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088 Throughput test setup</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088-Throughput-test-setup/m-p/1412953#M10034</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The numbers specified in the DPAA2 Low-level hardware reference manual are the maximum values for the&amp;nbsp; WRIOP engine version present in&amp;nbsp; LS1088.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Feb 2022 08:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088-Throughput-test-setup/m-p/1412953#M10034</guid>
      <dc:creator>andrei_skok</dc:creator>
      <dc:date>2022-02-14T08:12:14Z</dc:date>
    </item>
  </channel>
</rss>