<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C Slave detect Repeated Start in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1410835#M10017</link>
    <description>&lt;P&gt;I clearly understand the situation you are describing.&lt;/P&gt;&lt;P&gt;I'd hope that the first slave device would ignore the transaction with the second slave device (that's what I2C addresses are for, right) and thus keep its internal state machine (unaffected by the transaction with the second slave). But I don't know for sure whether I2C supports these kind of "piecewise" transactions.&lt;/P&gt;&lt;P&gt;Therefore I wonder why there's no reply from NXP. I'd be happy to have an official view on this situation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Feb 2022 08:57:23 GMT</pubDate>
    <dc:creator>danielholala</dc:creator>
    <dc:date>2022-02-09T08:57:23Z</dc:date>
    <item>
      <title>I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237218#M7601</link>
      <description>&lt;P&gt;If a Master I2C device is communicating with a Slave I2C device and generates a Repeated Start condition and starts communicating with second Slave I2C device, how will the first Slave device detect the Repeated Start condition? Will it be able to detect the Repeated Start at all, or will it keep waiting until the Master addresses it again?&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 09:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237218#M7601</guid>
      <dc:creator>gauthamkrishnan_r</dc:creator>
      <dc:date>2021-02-26T09:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237719#M7604</link>
      <description>&lt;P&gt;The I2C specs says:&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;I2&lt;/SPAN&gt;&lt;SPAN class="fontstyle0"&gt;C-bus compatible devices must reset their bus logic on receipt of a START or repeated START condition such that they all anticipate the sending of a slave address, even if these START conditions are not positioned according to the proper format.&lt;/SPAN&gt; &lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 05:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237719#M7604</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2021-03-01T05:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237750#M7605</link>
      <description>&lt;P&gt;Does it mean my slave device will not be able to recognize that the Master has started communicating to another slave device using a Repeated Start?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 06:48:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237750#M7605</guid>
      <dc:creator>gauthamkrishnan_r</dc:creator>
      <dc:date>2021-03-01T06:48:48Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237782#M7606</link>
      <description>&lt;P&gt;It means that &lt;SPAN class="fontstyle0"&gt;a START condition and repeated START condition treated in the same way and the slave address will be checked.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 07:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237782#M7606</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2021-03-01T07:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237864#M7608</link>
      <description>&lt;P&gt;Agree, but what will be the effect of the Repeated Start on the first slave device once the Master starts communicating with second slave device? The communication with first slave device is not cleanly terminated.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Mar 2021 09:26:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1237864#M7608</guid>
      <dc:creator>gauthamkrishnan_r</dc:creator>
      <dc:date>2021-03-01T09:26:57Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1240667#M7621</link>
      <description>&lt;P&gt;What do you mean as communication with first slave device is clearly terminated? How it should be done?&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 03:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1240667#M7621</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2021-03-05T03:36:12Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1240691#M7622</link>
      <description>&lt;P&gt;I mean a 'clean termination' is done by a Stop condition, but in the absence of a Stop condition to the first slave device (when master initiates a Repeated Start followed by slave address of another slave device), the first slave device will not be able to recognize that master's communication with it has ended.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 04:40:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1240691#M7622</guid>
      <dc:creator>gauthamkrishnan_r</dc:creator>
      <dc:date>2021-03-05T04:40:21Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Slave detect Repeated Start</title>
      <link>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1410835#M10017</link>
      <description>&lt;P&gt;I clearly understand the situation you are describing.&lt;/P&gt;&lt;P&gt;I'd hope that the first slave device would ignore the transaction with the second slave device (that's what I2C addresses are for, right) and thus keep its internal state machine (unaffected by the transaction with the second slave). But I don't know for sure whether I2C supports these kind of "piecewise" transactions.&lt;/P&gt;&lt;P&gt;Therefore I wonder why there's no reply from NXP. I'd be happy to have an official view on this situation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 08:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/I2C-Slave-detect-Repeated-Start/m-p/1410835#M10017</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2022-02-09T08:57:23Z</dc:date>
    </item>
  </channel>
</rss>