<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046A DPAA Jumbo Frame using upstream ethernet driver in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409601#M10006</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes this procedure is the one that should work when using private driver. I choose to use mainline driver, so these are either not available (CONFIG_FSL_FM_MAX_FRAME_SIZE), or doesn't work (fsl_fm_max_frm=9600 in kernel's command line).&lt;/P&gt;&lt;P&gt;I see that I could create a new devicetree value (like max_l2_size) and modify fman driver to use it, but I was wondering why jumbo frame was not available as is in mainline driver.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Frederic.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Feb 2022 10:08:47 GMT</pubDate>
    <dc:creator>fredericlefranc</dc:creator>
    <dc:date>2022-02-07T10:08:47Z</dc:date>
    <item>
      <title>LS1046A DPAA Jumbo Frame using upstream ethernet driver</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409098#M9993</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using the linux kernel from LSDK_21_08 (kernel 5.10). I choose to use DPAA upstream driver instead of the private one.&lt;/P&gt;&lt;P&gt;Everything is working properly except the fact that I can't change MTU to something bigger than the default 1500.&lt;/P&gt;&lt;P&gt;I've tried to use the max-frame-size property in the device tree for each ethernet, but it doesn't change anything.&lt;BR /&gt;It seems that to achieve a higher MTU value, I need to configure frame size in FMAN, but with the upstream driver, I have no way to do that.&lt;/P&gt;&lt;P&gt;Do you guys have a solution to allow jumbo frames on LS1046A using upstream driver?&lt;/P&gt;&lt;P&gt;Side question, what are the advantages/disadvantages of using private driver instead of mainline one?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Fred.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Feb 2022 16:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409098#M9993</guid>
      <dc:creator>fredericlefranc</dc:creator>
      <dc:date>2022-02-04T16:35:03Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DPAA Jumbo Frame using upstream ethernet driver</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409494#M10004</link>
      <description>&lt;P&gt;To enable Jumbo frame, the user is required to set the L2 maximum frame size to 9600, otherwise the configuration is not valid.&lt;/P&gt;&lt;P&gt;This can be achieved by either setting fsl_fm_max_frm=9600 in the bootargs, or configuring CONFIG_FSL_FM_MAX_FRAME_SIZE from menuconfig.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 07:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409494#M10004</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-02-07T07:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DPAA Jumbo Frame using upstream ethernet driver</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409601#M10006</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes this procedure is the one that should work when using private driver. I choose to use mainline driver, so these are either not available (CONFIG_FSL_FM_MAX_FRAME_SIZE), or doesn't work (fsl_fm_max_frm=9600 in kernel's command line).&lt;/P&gt;&lt;P&gt;I see that I could create a new devicetree value (like max_l2_size) and modify fman driver to use it, but I was wondering why jumbo frame was not available as is in mainline driver.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Frederic.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Feb 2022 10:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1409601#M10006</guid>
      <dc:creator>fredericlefranc</dc:creator>
      <dc:date>2022-02-07T10:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A DPAA Jumbo Frame using upstream ethernet driver</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1498528#M10967</link>
      <description>&lt;P&gt;I am experiencing this same problem with the DPAA/FMAN drivers in the mainline kernel. I am using linux-5.18 kernel. So the problem still exits as far as I can tell.&lt;/P&gt;&lt;P&gt;Federic, did you ever get a solution to fix this on mainline kernels?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 05:55:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-DPAA-Jumbo-Frame-using-upstream-ethernet-driver/m-p/1498528#M10967</guid>
      <dc:creator>GregUngerer1</dc:creator>
      <dc:date>2022-08-01T05:55:45Z</dc:date>
    </item>
  </channel>
</rss>