<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Implementing AI/ML on KW45B41Z-EVK in Generative AI &amp; LLMs</title>
    <link>https://community.nxp.com/t5/Generative-AI-LLMs/Implementing-AI-ML-on-KW45B41Z-EVK/m-p/2412109#M33</link>
    <description>&lt;P lang="es-419"&gt;Hello, hope you are doing well.&lt;/P&gt;
&lt;P&gt;If you are using eIQ Time Series Studio (TSS), I would recommend porting your project from the FRDM-MCXW71 instead. It is an officially supported target in eIQ TSS and is software compatible with the KW45. Both devices share the same Cortex-M33 core architecture and a similar memory profile, so the generated library should be a much closer match for your hardware.&lt;/P&gt;
&lt;P&gt;When using a device with such a different hardware profile as the FRDM-MCXN947 as a target for porting, there is a risk of generating incompatible models, for example, due to the differences in available RAM between both devices, or the generation of NPU-accelerated models specific to the MCXN947.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Sep 2026 17:41:14 GMT</pubDate>
    <dc:creator>sofiaurueta</dc:creator>
    <dc:date>2026-09-08T17:41:14Z</dc:date>
    <item>
      <title>Implementing AI/ML on KW45B41Z-EVK</title>
      <link>https://community.nxp.com/t5/Generative-AI-LLMs/Implementing-AI-ML-on-KW45B41Z-EVK/m-p/2411360#M31</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hi NXP Community,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am working on an edge AI application for the&amp;nbsp;&lt;STRONG&gt;KW45B41Z-EVK&lt;/STRONG&gt;&amp;nbsp;(Cortex-M33)&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;and would like advice on deploying a machine learning model on this board&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Since the KW45 SDK does not include the eIQ/TFLM middleware by default&lt;/SPAN&gt;&lt;SPAN&gt;, my plan is:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;Model Training:&lt;/STRONG&gt;&amp;nbsp;Train an n-class classification model for time-series data using&amp;nbsp;&lt;STRONG&gt;eIQ Time Series Studio (eIQ TSS)&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN&gt;. Since the KW45 is not listed as a target in eIQ TSS, I selected the&amp;nbsp;&lt;STRONG&gt;FRDM-MCXN947&lt;/STRONG&gt;&amp;nbsp;(Cortex-M33) as the target platform to export the model&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;Runtime Deployment:&lt;/STRONG&gt;&amp;nbsp;Port the middleware/eiq/tensorflow-lite folder from the&amp;nbsp;&lt;STRONG&gt;FRDM-MCXN947 SDK&lt;/STRONG&gt;&amp;nbsp;into my KW45 SDK project and link it with CMSIS-NN&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;My Questions:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;Is porting the eIQ TFLM middleware from the MCXN947 SDK to the KW45 SDK a valid and supported approach&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;Is selecting the FRDM-MCXN947 in eIQ TSS suitable for generating models to run on the KW45&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN&gt;Is there any other recommended or native workflow to implement AI/ML on the KW45B41Z-EVK&lt;/SPAN&gt;&lt;SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Thanks for your help!&lt;BR /&gt;&lt;LI-PRODUCT title="KW45B41Z-EVK" id="KW45B41Z-EVK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="KW45" id="KW45"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="EIQ-TFLITE-MICRO" id="EIQ-TFLITE-MICRO"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="EIQ-TOOLKIT" id="EIQ-TOOLKIT"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;#AIML&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2026 12:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Generative-AI-LLMs/Implementing-AI-ML-on-KW45B41Z-EVK/m-p/2411360#M31</guid>
      <dc:creator>Srushti_Mulimani</dc:creator>
      <dc:date>2026-09-04T12:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing AI/ML on KW45B41Z-EVK</title>
      <link>https://community.nxp.com/t5/Generative-AI-LLMs/Implementing-AI-ML-on-KW45B41Z-EVK/m-p/2412109#M33</link>
      <description>&lt;P lang="es-419"&gt;Hello, hope you are doing well.&lt;/P&gt;
&lt;P&gt;If you are using eIQ Time Series Studio (TSS), I would recommend porting your project from the FRDM-MCXW71 instead. It is an officially supported target in eIQ TSS and is software compatible with the KW45. Both devices share the same Cortex-M33 core architecture and a similar memory profile, so the generated library should be a much closer match for your hardware.&lt;/P&gt;
&lt;P&gt;When using a device with such a different hardware profile as the FRDM-MCXN947 as a target for porting, there is a risk of generating incompatible models, for example, due to the differences in available RAM between both devices, or the generation of NPU-accelerated models specific to the MCXN947.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2026 17:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Generative-AI-LLMs/Implementing-AI-ML-on-KW45B41Z-EVK/m-p/2412109#M33</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2026-09-08T17:41:14Z</dc:date>
    </item>
  </channel>
</rss>