<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to compile gui guider project as dll in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/How-to-compile-gui-guider-project-as-dll/m-p/1860391#M955</link>
    <description>&lt;P&gt;I have to import gui guider project in an mcuxpresso project. I now have a complicated procedure that utilizes python script to copy necessary files to the project. It would be very useful to me if I could compile the gui guider project as a dll and then simply include it in my project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can also be useful if I have multiple gui's, where I can flash multiple dll's and then the app will load them on runtime based on which gui is needed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case that it isn't possible now to do it, I would like to make an appeal to include this funcitonality in the next version.&lt;/P&gt;</description>
    <pubDate>Tue, 07 May 2024 09:10:43 GMT</pubDate>
    <dc:creator>bosnian_beast</dc:creator>
    <dc:date>2024-05-07T09:10:43Z</dc:date>
    <item>
      <title>How to compile gui guider project as dll</title>
      <link>https://community.nxp.com/t5/GUI-Guider/How-to-compile-gui-guider-project-as-dll/m-p/1860391#M955</link>
      <description>&lt;P&gt;I have to import gui guider project in an mcuxpresso project. I now have a complicated procedure that utilizes python script to copy necessary files to the project. It would be very useful to me if I could compile the gui guider project as a dll and then simply include it in my project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can also be useful if I have multiple gui's, where I can flash multiple dll's and then the app will load them on runtime based on which gui is needed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case that it isn't possible now to do it, I would like to make an appeal to include this funcitonality in the next version.&lt;/P&gt;</description>
      <pubDate>Tue, 07 May 2024 09:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/How-to-compile-gui-guider-project-as-dll/m-p/1860391#M955</guid>
      <dc:creator>bosnian_beast</dc:creator>
      <dc:date>2024-05-07T09:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: How to compile gui guider project as dll</title>
      <link>https://community.nxp.com/t5/GUI-Guider/How-to-compile-gui-guider-project-as-dll/m-p/1860833#M957</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206746"&gt;@bosnian_beast&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This is not possible on the current version of GUI Guider, but I will relay your suggestion to the GUI Guider team in order for them to discuss and hopefully add on a future release of the Tool. It would be a great thing to add to GUI Guider.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 07 May 2024 21:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/How-to-compile-gui-guider-project-as-dll/m-p/1860833#M957</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-05-07T21:56:46Z</dc:date>
    </item>
  </channel>
</rss>