<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GUI Guider bug report in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1294671#M8</link>
    <description>&lt;P&gt;GUI Guider bug report&lt;/P&gt;
&lt;P&gt;Hello all,&lt;/P&gt;
&lt;P&gt;The customer (original cases #00374019 and #00374024 in SFDC) reports a bugs in &lt;BR /&gt;the GUI Guider software. Below is the customer's messages.&lt;/P&gt;
&lt;P&gt;"See the attached figure.&lt;BR /&gt;When LINE CAP = butt is set in "arc" widgets, the edge display of Active (white) becomes a straight line.&lt;BR /&gt;However, the edge display of Backgroud (yellow) remains round. Is this a bug?&lt;BR /&gt;* Because the semicircle remains yellow at the start position.&lt;BR /&gt;This time, the customer wants to use a straight line both inside and outside the curve.&lt;/P&gt;
&lt;P&gt;By the way, the latest version of Gui Guider is 1.1.0.&lt;/P&gt;
&lt;P&gt;In the previous 1.0.0, it was a straight line as intended on the GUI, but when it was displayed on the Simulator and the actual board, it became a circle."&lt;/P&gt;
&lt;P&gt;"Regarding Gui Guider, if the line is thickened as shown in the attachment, the display will be misaligned on the Simulator and GUI.&lt;BR /&gt;Is this a bug?&lt;BR /&gt;* The left is the layout on the GUI, and the right is the display on the Simulator.&lt;/P&gt;
&lt;P&gt;The customer's environment is as follows.&lt;/P&gt;
&lt;P&gt;· MCU to be used&lt;/P&gt;
&lt;P&gt;I.MX RT1064&lt;/P&gt;
&lt;P&gt;· GUI Guider&lt;/P&gt;
&lt;P&gt;Version 1.1.0-GA&lt;/P&gt;
&lt;P&gt;· Windows&lt;/P&gt;
&lt;P&gt;Windows 10 pro&lt;/P&gt;
&lt;P&gt;Version 1909&lt;/P&gt;
&lt;P&gt;System type&lt;/P&gt;
&lt;P&gt;64-bit operating system, x64-based processor&lt;/P&gt;
&lt;P&gt;· MCUXpresso IDE&lt;/P&gt;
&lt;P&gt;V11.3.1 [build 5262] [2021-04-02]&lt;/P&gt;
&lt;P&gt;· SDK_2x_EVK-MIMRT1064&lt;/P&gt;
&lt;P&gt;Version 2.9.2&lt;/P&gt;
&lt;P&gt;Manifest Version 3.8.0&lt;/P&gt;
&lt;P&gt;So, can someone please check/fix the issues above?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
    <pubDate>Fri, 18 Jun 2021 11:34:22 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2021-06-18T11:34:22Z</dc:date>
    <item>
      <title>GUI Guider bug report</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1294671#M8</link>
      <description>&lt;P&gt;GUI Guider bug report&lt;/P&gt;
&lt;P&gt;Hello all,&lt;/P&gt;
&lt;P&gt;The customer (original cases #00374019 and #00374024 in SFDC) reports a bugs in &lt;BR /&gt;the GUI Guider software. Below is the customer's messages.&lt;/P&gt;
&lt;P&gt;"See the attached figure.&lt;BR /&gt;When LINE CAP = butt is set in "arc" widgets, the edge display of Active (white) becomes a straight line.&lt;BR /&gt;However, the edge display of Backgroud (yellow) remains round. Is this a bug?&lt;BR /&gt;* Because the semicircle remains yellow at the start position.&lt;BR /&gt;This time, the customer wants to use a straight line both inside and outside the curve.&lt;/P&gt;
&lt;P&gt;By the way, the latest version of Gui Guider is 1.1.0.&lt;/P&gt;
&lt;P&gt;In the previous 1.0.0, it was a straight line as intended on the GUI, but when it was displayed on the Simulator and the actual board, it became a circle."&lt;/P&gt;
&lt;P&gt;"Regarding Gui Guider, if the line is thickened as shown in the attachment, the display will be misaligned on the Simulator and GUI.&lt;BR /&gt;Is this a bug?&lt;BR /&gt;* The left is the layout on the GUI, and the right is the display on the Simulator.&lt;/P&gt;
&lt;P&gt;The customer's environment is as follows.&lt;/P&gt;
&lt;P&gt;· MCU to be used&lt;/P&gt;
&lt;P&gt;I.MX RT1064&lt;/P&gt;
&lt;P&gt;· GUI Guider&lt;/P&gt;
&lt;P&gt;Version 1.1.0-GA&lt;/P&gt;
&lt;P&gt;· Windows&lt;/P&gt;
&lt;P&gt;Windows 10 pro&lt;/P&gt;
&lt;P&gt;Version 1909&lt;/P&gt;
&lt;P&gt;System type&lt;/P&gt;
&lt;P&gt;64-bit operating system, x64-based processor&lt;/P&gt;
&lt;P&gt;· MCUXpresso IDE&lt;/P&gt;
&lt;P&gt;V11.3.1 [build 5262] [2021-04-02]&lt;/P&gt;
&lt;P&gt;· SDK_2x_EVK-MIMRT1064&lt;/P&gt;
&lt;P&gt;Version 2.9.2&lt;/P&gt;
&lt;P&gt;Manifest Version 3.8.0&lt;/P&gt;
&lt;P&gt;So, can someone please check/fix the issues above?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Artur&lt;/P&gt;</description>
      <pubDate>Fri, 18 Jun 2021 11:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1294671#M8</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2021-06-18T11:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider bug report</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1296828#M11</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Artur,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please see my comments of the 2 issues.&lt;/P&gt;
&lt;P&gt;1. “LINE CAP = butt” of arc widget only applies for the edge display of Active part, the edge display of Background doesn’t apply.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is a bug of GG, we will fix it in next release, the following line can be added in&amp;nbsp;setup_scr_screen.c to workaround the issue, please replace the first parameter with actual widget name.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;lv_obj_set_style_local_line_rounded(ui-&amp;gt;screen_arc_1, LV_ARC_PART_BG, LV_STATE_DEFAULT, 0);&lt;/P&gt;
&lt;P&gt;2. When the line is thickened, the display will be misaligned on the Simulator and GUI.&lt;/P&gt;
&lt;P&gt;This is a bug of GG, it will be fixed in new GG release.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Zhenhua&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 11:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1296828#M11</guid>
      <dc:creator>zhenhualuo</dc:creator>
      <dc:date>2021-06-23T11:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider bug report</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1325340#M16</link>
      <description>&lt;P&gt;The two bugs are fixed in GUI Guider v1.2.0 release, the new version can be downloaded from&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER" target="_blank"&gt;https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/153323i2D1F3D28220FBC77/image-size/medium?v=v2&amp;amp;px=400" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Wed, 18 Aug 2021 08:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-bug-report/m-p/1325340#M16</guid>
      <dc:creator>zhenhualuo</dc:creator>
      <dc:date>2021-08-18T08:56:02Z</dc:date>
    </item>
  </channel>
</rss>