<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI GuiderのトピックRe: Arduino IDE and LGVL Function</title>
    <link>https://community.nxp.com/t5/GUI-Guider/Arduino-IDE-and-LGVL-Function/m-p/1744959#M541</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that it is a large project to port the LVGL to Arduino IDE.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
    <pubDate>Tue, 24 Oct 2023 03:20:35 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2023-10-24T03:20:35Z</dc:date>
    <item>
      <title>Arduino IDE and LGVL Function</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Arduino-IDE-and-LGVL-Function/m-p/1743078#M532</link>
      <description>&lt;P&gt;I would like to export the GUI BUILDER files and use them in the Arduino IDE.&lt;/P&gt;&lt;P&gt;Which lvgl function do I call to initialize the app made in the GUI Builder?&lt;/P&gt;&lt;P&gt;What files do I have to change considering that in the Arduino IDE I need to have all the files in the same directory without folders and subfolders?&lt;/P&gt;&lt;P&gt;Could anyone help me in this regard?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Oct 2023 16:12:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Arduino-IDE-and-LGVL-Function/m-p/1743078#M532</guid>
      <dc:creator>allacmc</dc:creator>
      <dc:date>2023-10-19T16:12:51Z</dc:date>
    </item>
    <item>
      <title>Re: Arduino IDE and LGVL Function</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Arduino-IDE-and-LGVL-Function/m-p/1744959#M541</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I suppose that it is a large project to port the LVGL to Arduino IDE.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun rong&lt;/P&gt;</description>
      <pubDate>Tue, 24 Oct 2023 03:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Arduino-IDE-and-LGVL-Function/m-p/1744959#M541</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2023-10-24T03:20:35Z</dc:date>
    </item>
  </channel>
</rss>