<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GUI Guider with bare metal in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379374#M54</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently GUI Guider supports build-in FreeRTOS-based build and deploy for target board, the source code exported BY GUI Guider doesn't depend on FreeRTOS, it can support bare-metal usage.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Zhenhua&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Dec 2021 05:36:31 GMT</pubDate>
    <dc:creator>zhenhualuo</dc:creator>
    <dc:date>2021-12-01T05:36:31Z</dc:date>
    <item>
      <title>GUI Guider with bare metal</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379185#M50</link>
      <description>&lt;P&gt;I'm working on a GUI project and was planning to use LVGL which i know can run without an OS. My project is not complex so Id rather start without an OS. I wanted to use GUI Guider to speed up development but the options (I'm using mimxrt1050-evkb) show the OS as FreeRTOS. My questions are:&lt;BR /&gt;If I wish to incorporate the generated code into a project will it have FreeRTOS dependencies?&lt;BR /&gt;If so, can I set up GUI Guider so not use an OS?&lt;BR /&gt;&lt;BR /&gt;Not the end of the world but would like to avoid OS is possible lol&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 30 Nov 2021 20:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379185#M50</guid>
      <dc:creator>BabyBorisova</dc:creator>
      <dc:date>2021-11-30T20:23:41Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider with bare metal</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379368#M53</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Have a look at the following stuff&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/gertvb/LPC55S69_GuiGuider" target="_blank"&gt;https://github.com/gertvb/LPC55S69_GuiGuider&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically gui guider on a bare metal lpc55s69&lt;/P&gt;</description>
      <pubDate>Wed, 01 Dec 2021 05:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379368#M53</guid>
      <dc:creator>gertvb</dc:creator>
      <dc:date>2021-12-01T05:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider with bare metal</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379374#M54</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently GUI Guider supports build-in FreeRTOS-based build and deploy for target board, the source code exported BY GUI Guider doesn't depend on FreeRTOS, it can support bare-metal usage.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Zhenhua&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Dec 2021 05:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1379374#M54</guid>
      <dc:creator>zhenhualuo</dc:creator>
      <dc:date>2021-12-01T05:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider with bare metal</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1380110#M56</link>
      <description>&lt;P&gt;Hey&amp;nbsp;&lt;SPAN&gt;Zhenhua,&lt;BR /&gt;&lt;BR /&gt;Thanks for such a quick response. I've tested and looked through the generated code and understand how it works now. Its good to know that FreeRTOS is nota requirement of the generated code so i can continue with my work.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Kind regards and my thanks,&lt;BR /&gt;Lexi&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Dec 2021 00:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-with-bare-metal/m-p/1380110#M56</guid>
      <dc:creator>BabyBorisova</dc:creator>
      <dc:date>2021-12-02T00:48:07Z</dc:date>
    </item>
  </channel>
</rss>