<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic To dumb on a TFT disply in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/m-p/1714007#M442</link>
    <description>&lt;P&gt;the examples from gui guider is perfectly working on the rt1170 evk board , but im having the same board with an another display(RGB TFT Display (800*480)), what changes i have to made in the current working code which is suitable for the on-board display of evk board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 11:48:21 GMT</pubDate>
    <dc:creator>sajithdevidas</dc:creator>
    <dc:date>2023-08-30T11:48:21Z</dc:date>
    <item>
      <title>To dumb on a TFT disply</title>
      <link>https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/m-p/1714007#M442</link>
      <description>&lt;P&gt;the examples from gui guider is perfectly working on the rt1170 evk board , but im having the same board with an another display(RGB TFT Display (800*480)), what changes i have to made in the current working code which is suitable for the on-board display of evk board&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 11:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/m-p/1714007#M442</guid>
      <dc:creator>sajithdevidas</dc:creator>
      <dc:date>2023-08-30T11:48:21Z</dc:date>
    </item>
    <item>
      <title>Re: To dumb on a TFT disply</title>
      <link>https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/m-p/1714560#M444</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;sajithdevidas,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;you can create a project using the custom panel like screenshot1, then go to the&amp;nbsp;&amp;lt;project folder&amp;gt;\sdk\Core\board folder and edit the&amp;nbsp;display_support.c/h file to add display config for your panel like&amp;nbsp;screenshot2.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Zongchun&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Aug 2023 02:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/To-dumb-on-a-TFT-disply/m-p/1714560#M444</guid>
      <dc:creator>zongchunyu</dc:creator>
      <dc:date>2023-08-31T02:35:36Z</dc:date>
    </item>
  </channel>
</rss>