<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI GuiderのトピックCalling a custom Function</title>
    <link>https://community.nxp.com/t5/GUI-Guider/Calling-a-custom-Function/m-p/1709884#M436</link>
    <description>&lt;P&gt;i wrote a function inside custom.c, for the continuos movement of meter needle, how can i call the function repeatedly, i called the function in main while loop, the function is calling repeatedly but it does not shows any changes in the display, but while calling the function using timer handler its working fine, but using timer handler the function is calling with very less frequency, even i created a timer using 'lv_timer_creatre", and gave 10 ms period, then also the function is calling after 100ms only,&lt;/P&gt;&lt;P&gt;How can i call my custom function in while loop, is there any another methode is available?&lt;/P&gt;&lt;P&gt;im using rt1170evk board with gui guider&lt;/P&gt;</description>
    <pubDate>Wed, 23 Aug 2023 11:48:02 GMT</pubDate>
    <dc:creator>sajithdevidas</dc:creator>
    <dc:date>2023-08-23T11:48:02Z</dc:date>
    <item>
      <title>Calling a custom Function</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Calling-a-custom-Function/m-p/1709884#M436</link>
      <description>&lt;P&gt;i wrote a function inside custom.c, for the continuos movement of meter needle, how can i call the function repeatedly, i called the function in main while loop, the function is calling repeatedly but it does not shows any changes in the display, but while calling the function using timer handler its working fine, but using timer handler the function is calling with very less frequency, even i created a timer using 'lv_timer_creatre", and gave 10 ms period, then also the function is calling after 100ms only,&lt;/P&gt;&lt;P&gt;How can i call my custom function in while loop, is there any another methode is available?&lt;/P&gt;&lt;P&gt;im using rt1170evk board with gui guider&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 11:48:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Calling-a-custom-Function/m-p/1709884#M436</guid>
      <dc:creator>sajithdevidas</dc:creator>
      <dc:date>2023-08-23T11:48:02Z</dc:date>
    </item>
    <item>
      <title>Re: Calling a custom Function</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Calling-a-custom-Function/m-p/1711610#M437</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222022"&gt;@sajithdevidas&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please take a look at the following information?&lt;/P&gt;
&lt;UL class="lia-align-justify" type="disc"&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.jp/docs/en/user-guide/GUI_Guider_User_Manual.pdf" target="_blank"&gt;GUI Guider User's Guide&lt;/A&gt;,&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_self"&gt;RT1170EVK SDK's examples&lt;/A&gt;, and&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/design/software/development-software/gui-guider:GUI-GUIDER" target="_self"&gt;Gui Guider v1.6 GA templates&lt;/A&gt;.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P class="lia-align-justify"&gt;It might be useful to look at.&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Fri, 25 Aug 2023 18:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Calling-a-custom-Function/m-p/1711610#M437</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-08-25T18:44:01Z</dc:date>
    </item>
  </channel>
</rss>