<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: guider can't  edit code in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/guider-can-t-edit-code/m-p/1629533#M317</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215391"&gt;@susan1999&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks so much for your suggestions, I will forward them to development team, thanks!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
    <pubDate>Fri, 07 Apr 2023 06:26:10 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2023-04-07T06:26:10Z</dc:date>
    <item>
      <title>guider can't  edit code</title>
      <link>https://community.nxp.com/t5/GUI-Guider/guider-can-t-edit-code/m-p/1628868#M315</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;i'm using 1.5.0, fond some question:&lt;/P&gt;&lt;P&gt;1.image no rotate animation,and rotation center offset;&lt;/P&gt;&lt;P&gt;2.code viewer only for view,can't edit code,&amp;nbsp;this is a significant flaw.&lt;/P&gt;&lt;P&gt;becauce if want to click a button another image move or rotate.GUIder&amp;nbsp;unable to achieve.&lt;/P&gt;&lt;P&gt;so the two button&amp;nbsp;functions should be modified:&lt;/P&gt;&lt;P&gt;[Generate Code] only generate code;&lt;/P&gt;&lt;P&gt;[Simulator] only build and run (do not generate);&lt;/P&gt;&lt;P&gt;then,i can generate code if i need, or i can edit code to do some thing that GUIder not achieved;&lt;/P&gt;&lt;P&gt;I hope to do everything well in the GUIder and see the simulation run,then migrate to other devices.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 07:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/guider-can-t-edit-code/m-p/1628868#M315</guid>
      <dc:creator>susan1999</dc:creator>
      <dc:date>2023-04-06T07:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: guider can't  edit code</title>
      <link>https://community.nxp.com/t5/GUI-Guider/guider-can-t-edit-code/m-p/1629533#M317</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215391"&gt;@susan1999&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks so much for your suggestions, I will forward them to development team, thanks!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 06:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/guider-can-t-edit-code/m-p/1629533#M317</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-04-07T06:26:10Z</dc:date>
    </item>
  </channel>
</rss>