<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI Guider中的主题 Re: v1.5 Speedometer example, Custom Resolution 320x170 Micropython renders wrongly</title>
    <link>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1587863#M223</link>
    <description>&lt;P&gt;hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211541"&gt;@tyeth&lt;/a&gt; we release a new version of Gui Guider, you can test it and if your error has disappeared, if not, could you give us more information about your board that are you using, MCU, and what is the problem about the MCU and GuiGuider?&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jan 2023 18:43:44 GMT</pubDate>
    <dc:creator>CarlosGarabito</dc:creator>
    <dc:date>2023-01-25T18:43:44Z</dc:date>
    <item>
      <title>v1.5 Speedometer example, Custom Resolution 320x170 Micropython renders wrongly</title>
      <link>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1586352#M217</link>
      <description>&lt;P&gt;Create a new simulator project, with the device resolution set to 320x170&lt;/P&gt;&lt;P&gt;Select the example of Speedometer template when offered.&lt;/P&gt;&lt;P&gt;Run the example as micropython code and agree to autogeneration.&lt;/P&gt;&lt;P&gt;Notice the speed label is truncated by the units label, and on the graph page the vertical axis is messed up / truncated. The button label is also incorrectly laid out.&lt;/P&gt;&lt;P&gt;Run the same project as a C project, accept the autogenerated code, and then notice the demo looks as expected, matching the expectations from the designer or from LVGL more closely.&lt;/P&gt;</description>
      <pubDate>Sat, 21 Jan 2023 16:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1586352#M217</guid>
      <dc:creator>tyeth</dc:creator>
      <dc:date>2023-01-21T16:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: v1.5 Speedometer example, Custom Resolution 320x170 Micropython renders wrongly</title>
      <link>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1586760#M219</link>
      <description>&lt;P&gt;Can you tell us which MCU are you using please?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 17:59:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1586760#M219</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-23T17:59:56Z</dc:date>
    </item>
    <item>
      <title>Re: v1.5 Speedometer example, Custom Resolution 320x170 Micropython renders wrongly</title>
      <link>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1587863#M223</link>
      <description>&lt;P&gt;hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211541"&gt;@tyeth&lt;/a&gt; we release a new version of Gui Guider, you can test it and if your error has disappeared, if not, could you give us more information about your board that are you using, MCU, and what is the problem about the MCU and GuiGuider?&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 18:43:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1587863#M223</guid>
      <dc:creator>CarlosGarabito</dc:creator>
      <dc:date>2023-01-25T18:43:44Z</dc:date>
    </item>
    <item>
      <title>Re: v1.5 Speedometer example, Custom Resolution 320x170 Micropython renders wrongly</title>
      <link>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1590968#M224</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211541"&gt;@tyeth&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;This issue is caused by different&amp;nbsp;font size between C and MicroPython simulator, there're 2 suggestions for you:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Don't choose a resolution that differ significantly from default resolution(480 * 272) when use MicroPython simulator.&lt;/LI&gt;
&lt;LI&gt;Modify attributes of all labels after when you use MicroPython as major language.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Thank you for your feedback!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Wenbin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Feb 2023 04:05:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/v1-5-Speedometer-example-Custom-Resolution-320x170-Micropython/m-p/1590968#M224</guid>
      <dc:creator>WenbinYuan</dc:creator>
      <dc:date>2023-02-01T04:05:49Z</dc:date>
    </item>
  </channel>
</rss>