<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI GuiderのトピックRe: Unable to Run GUI Guider 1.10.0 DemoAPP on MIMXRT1170-EVKB</title>
    <link>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2190462#M1677</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have identified the root cause of the problem.&lt;BR /&gt;On the MIMXRT1170-EVKB board, pins 5 and 6 of the SDRAM (U25) were shorted, which prevented proper programming.&lt;/P&gt;&lt;P&gt;After removing the solder that caused the short and reprogramming the board, everything is now working correctly.&lt;/P&gt;&lt;P&gt;Thank you for your advice and support!&lt;/P&gt;</description>
    <pubDate>Wed, 22 Oct 2025 05:57:09 GMT</pubDate>
    <dc:creator>NXTyam</dc:creator>
    <dc:date>2025-10-22T05:57:09Z</dc:date>
    <item>
      <title>Unable to Run GUI Guider 1.10.0 DemoAPP on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2188912#M1668</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi NXP.&lt;/SPAN&gt;&lt;BR /&gt;I am trying to run the ButtonCounter demo application using the following setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MIMXRT1170-EVKB + RK055AHD091&lt;/LI&gt;&lt;LI&gt;GUI Guider 1.10.0-GA&lt;/LI&gt;&lt;LI&gt;MCUXpresso 25.6.136&lt;/LI&gt;&lt;LI&gt;LVGL 9.2.1 / LVGL 8.3.10&lt;/LI&gt;&lt;LI&gt;SDK 25.09.00&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;However, even after executing Build &amp;amp; Run Target, the application does not work as expected.&lt;BR /&gt;Am I doing something wrong? I would greatly appreciate any advice or guidance.&lt;BR /&gt;For reference, here is the toolchain output:&lt;/P&gt;&lt;LI-CODE lang="javascript"&gt;Checking device connection...
Cleaning generated screen files...
Generating C code...
✓ Code generation completed!
Run CMake To Generate Makefile
-- TOOLCHAIN_DIR: C:/nxp/MCUXpressoIDE_25.6.136/ide/tools
-- BUILD_TYPE: flexspi_nor_sdram_release
-- TOOLCHAIN_DIR: C:/nxp/MCUXpressoIDE_25.6.136/ide/tools
-- BUILD_TYPE: flexspi_nor_sdram_release
-- The C compiler identification is GNU 14.2.1
-- The CXX compiler identification is GNU 14.2.1
-- The ASM compiler identification is GNU&lt;/LI-CODE&gt;&lt;P&gt;Thank you in advance for your support!&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 05:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2188912#M1668</guid>
      <dc:creator>NXTyam</dc:creator>
      <dc:date>2025-10-20T05:54:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Run GUI Guider 1.10.0 DemoAPP on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2189130#M1669</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255952"&gt;@NXTyam&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Please check your MIMXRT1170-EVKB development board settings:&lt;/P&gt;
&lt;P&gt;1: Is the RK055AHD091 screen correctly connected to the J48 of the MIMXRT1170-EVKB development board?&lt;BR /&gt;2: Is 5V power connected to MIMXRT1170-EVKB J43, and is J38 set to 1-2?&lt;/P&gt;
&lt;P&gt;Have you successfully run GUI Guider project before? I suggest confirming your hardware development environment and then trying to run the simplest demo again.&lt;/P&gt;
&lt;P&gt;Wish it helps you.&lt;BR /&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;BR /&gt;MayLiu&lt;/P&gt;</description>
      <pubDate>Mon, 20 Oct 2025 10:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2189130#M1669</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-10-20T10:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Run GUI Guider 1.10.0 DemoAPP on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2189538#M1674</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;BR /&gt;As shown in the image below, the connections appear to be correct, and J48, J43, and J38 are all properly configured.&lt;/P&gt;&lt;P&gt;I have never been able to successfully run a GUI Guider project.&lt;BR /&gt;None of the demo applications work as expected; they all result in the same issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Oct 2025 02:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2189538#M1674</guid>
      <dc:creator>NXTyam</dc:creator>
      <dc:date>2025-10-21T02:58:57Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Run GUI Guider 1.10.0 DemoAPP on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2190462#M1677</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239163"&gt;@mayliu1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have identified the root cause of the problem.&lt;BR /&gt;On the MIMXRT1170-EVKB board, pins 5 and 6 of the SDRAM (U25) were shorted, which prevented proper programming.&lt;/P&gt;&lt;P&gt;After removing the solder that caused the short and reprogramming the board, everything is now working correctly.&lt;/P&gt;&lt;P&gt;Thank you for your advice and support!&lt;/P&gt;</description>
      <pubDate>Wed, 22 Oct 2025 05:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2190462#M1677</guid>
      <dc:creator>NXTyam</dc:creator>
      <dc:date>2025-10-22T05:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to Run GUI Guider 1.10.0 DemoAPP on MIMXRT1170-EVKB</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2190464#M1678</link>
      <description>&lt;P&gt;Thanks&amp;nbsp; for your solution sharing.&lt;/P&gt;
&lt;P&gt;If you meet any issue in the future, welcome to create the new question post.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Oct 2025 06:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Unable-to-Run-GUI-Guider-1-10-0-DemoAPP-on-MIMXRT1170-EVKB/m-p/2190464#M1678</guid>
      <dc:creator>mayliu1</dc:creator>
      <dc:date>2025-10-22T06:04:23Z</dc:date>
    </item>
  </channel>
</rss>