<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GUI Guider examples Horizontal vs Vertical in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180999#M1659</link>
    <description>&lt;P&gt;Thank you. To be honest it seems to be that also in GUI Guider 1.10.0 there isn't a horizontal option 720x1280. Anyway it's not a problem. Thanks for confirmation that I'm doing the correct thing.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Francesco&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Oct 2025 06:44:07 GMT</pubDate>
    <dc:creator>SolitoFrancesco</dc:creator>
    <dc:date>2025-10-07T06:44:07Z</dc:date>
    <item>
      <title>GUI Guider examples Horizontal vs Vertical</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180461#M1657</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I noticed that if I open an example project for MIMXRT1170-EVK, the default settings seem to be for vertical display, but then all the pictures "are stretched". If instead I modify the Panel Type in a "custom" way (so I put the same panel name RK055MHD091) using width=1280 and height=720, the pictures are represented correctly as expected.&lt;/P&gt;&lt;P&gt;I would like to have a confirmation that this is the normal behavior or not (because to be honest I expect to get the example already working correctly in horizontal way, so my doubt is that I'm making something wrong on another setting of GUI Guider or in a HW setting of the evaluation board).&lt;/P&gt;&lt;P&gt;Thnak you and kind regards,&lt;/P&gt;&lt;P&gt;Francesco&lt;/P&gt;</description>
      <pubDate>Mon, 06 Oct 2025 09:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180461#M1657</guid>
      <dc:creator>SolitoFrancesco</dc:creator>
      <dc:date>2025-10-06T09:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider examples Horizontal vs Vertical</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180710#M1658</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255225"&gt;@SolitoFrancesco&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, this would be the method to use on versions of GUI Guider that don't have the option of 1280x720 natively.&lt;/P&gt;
&lt;P&gt;That said, I would like to add a recommendation to make sure you are using the latest version of GUI Guider (v1.10.0).&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 06 Oct 2025 17:24:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180710#M1658</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-06T17:24:38Z</dc:date>
    </item>
    <item>
      <title>Re: GUI Guider examples Horizontal vs Vertical</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180999#M1659</link>
      <description>&lt;P&gt;Thank you. To be honest it seems to be that also in GUI Guider 1.10.0 there isn't a horizontal option 720x1280. Anyway it's not a problem. Thanks for confirmation that I'm doing the correct thing.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Francesco&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 06:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-Guider-examples-Horizontal-vs-Vertical/m-p/2180999#M1659</guid>
      <dc:creator>SolitoFrancesco</dc:creator>
      <dc:date>2025-10-07T06:44:07Z</dc:date>
    </item>
  </channel>
</rss>