<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lv_conf.h is overwritten in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538008#M161</link>
    <description>What I noticed as I was writing the above, the code that uses the chart widget is custom file, not generated by gui guider.&lt;BR /&gt;I placed a chart widget on a screen and the define was enabled.&lt;BR /&gt;&lt;BR /&gt;Is there somewhere in the documentation that states this file is auto-generated? Is there a way to turn the auto-generation off?&lt;BR /&gt;--John</description>
    <pubDate>Fri, 14 Oct 2022 19:01:04 GMT</pubDate>
    <dc:creator>JohnDel</dc:creator>
    <dc:date>2022-10-14T19:01:04Z</dc:date>
    <item>
      <title>lv_conf.h is overwritten</title>
      <link>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1537988#M160</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a gui guider project developed under 1.3.0 and am trying to update it to run under 1.4.1.&lt;/P&gt;&lt;P&gt;There were some small issues with button text fonts being carried over properly but those were easily updated.&lt;/P&gt;&lt;P&gt;My main problem seems to be that each time I generate new code or run simulator (which generates new code), the lv_conf.h file is updated, overwritten with what seems to be some sort of default version of the file? Widgets that I am using get the define turned off. ex.&amp;nbsp;#define LV_USE_CHART 0&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 18:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1537988#M160</guid>
      <dc:creator>JohnDel</dc:creator>
      <dc:date>2022-10-14T18:10:18Z</dc:date>
    </item>
    <item>
      <title>Re: lv_conf.h is overwritten</title>
      <link>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538008#M161</link>
      <description>What I noticed as I was writing the above, the code that uses the chart widget is custom file, not generated by gui guider.&lt;BR /&gt;I placed a chart widget on a screen and the define was enabled.&lt;BR /&gt;&lt;BR /&gt;Is there somewhere in the documentation that states this file is auto-generated? Is there a way to turn the auto-generation off?&lt;BR /&gt;--John</description>
      <pubDate>Fri, 14 Oct 2022 19:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538008#M161</guid>
      <dc:creator>JohnDel</dc:creator>
      <dc:date>2022-10-14T19:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: lv_conf.h is overwritten</title>
      <link>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538450#M163</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;There are two questions:&lt;/P&gt;
&lt;P&gt;1. Could you please specify how to reproduce this problem? Please provide us step by step guide.&lt;/P&gt;
&lt;P&gt;2. Is this problem in&amp;nbsp;&lt;SPAN&gt;1.4.1 only or also exists in&amp;nbsp;1.3.0?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jun Zhang&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 08:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538450#M163</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-10-17T08:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: lv_conf.h is overwritten</title>
      <link>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538605#M165</link>
      <description>&lt;P&gt;this did not happen in 1.3&lt;/P&gt;&lt;P&gt;To reproduce:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Create a blank simulator project in 1.4.1&lt;/LI&gt;&lt;LI&gt;hit run simulator, blank project builds, all good&lt;/LI&gt;&lt;LI&gt;create a file in ./custom such as chart.c&lt;/LI&gt;&lt;LI&gt;add&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;#include "gui_guider.h"&lt;/P&gt;&lt;P&gt;static lv_obj_t *SweepChart_chart = NULL;&lt;/P&gt;&lt;P&gt;void MyChart( void );&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;void MyChart( void )&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;SweepChart_chart = lv_chart_create( guider_ui.screen, NULL );&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;run simulator, compile fails as it can't find lv_chart_create()&lt;/LI&gt;&lt;LI&gt;edit ./lvgl-simulator/lv_conf.h&lt;UL&gt;&lt;LI&gt;change&amp;nbsp;#define LV_USE_CHART 0&amp;nbsp;&lt;UL&gt;&lt;LI&gt;to&amp;nbsp;#define LV_USE_CHART 1&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;run simulator, compile fails again&lt;/LI&gt;&lt;LI&gt;refresh lv_conf.h. Define has changed back to 0&lt;/LI&gt;&lt;LI&gt;drop a chart widget on the screen&lt;/LI&gt;&lt;LI&gt;run simulator, compile now complete, define is set to 1&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;It seems to be more of an issue with 1.4.1? I don't think 1.3 has anything to do with the issue.&lt;/P&gt;&lt;P&gt;My workaround for now is to simply create a blank screen which will not be shown and add the screen and message box widgets and it works.&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 13:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1538605#M165</guid>
      <dc:creator>JohnDel</dc:creator>
      <dc:date>2022-10-17T13:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: lv_conf.h is overwritten</title>
      <link>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1539084#M167</link>
      <description>&lt;P&gt;HI&amp;nbsp;JohnDel&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is a new feature since GUI Guider v1.4.0.&amp;nbsp;lv_conf.h is automatically updated based on project configurations.&lt;/P&gt;
&lt;P&gt;Unfortunately there is no option can diable it. I will escalated this feature as a feature request to development team. Thanks for bringing the problem to our attention.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Jun Zhang&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 07:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/lv-conf-h-is-overwritten/m-p/1539084#M167</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2022-10-18T07:55:23Z</dc:date>
    </item>
  </channel>
</rss>