<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GUI-guider exception, Error: Image size out of limit. The width and height should not exceed 128 in GUI Guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506161#M138</link>
    <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205029"&gt;@lucky1&lt;/a&gt;, this is a bug in the tool probably made from the assumption that only the officially supported displays (with 1280 px max size) would be supported. The limitation will be removed in version 1.4.1 so that displays of any size can be supported properly. For now a workaround would be to split the image into two parts and create two image widgets.&lt;/P&gt;
&lt;P&gt;Thank you for reporting this issue.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Aug 2022 12:07:25 GMT</pubDate>
    <dc:creator>david_piskula</dc:creator>
    <dc:date>2022-08-15T12:07:25Z</dc:date>
    <item>
      <title>GUI-guider exception, Error: Image size out of limit. The width and height should not exceed 1280</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1505855#M131</link>
      <description>&lt;P&gt;GUI-guider1.4.0&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My asserts picture file resolution size 720x1440.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Run &lt;SPAN&gt;simulate&lt;/SPAN&gt; occur exception,as flows,&lt;/P&gt;&lt;LI-CODE lang="cpp"&gt;Uit 3.0: Start to generate C code for UI

Uit 3.0: Generate C code for screen
Uit 3.0: Generate C code for screen_img_1
Error: Image size out of limit. The width and height should not exceed 1280 ! color depth: 24 /Applications/Gui-Guider.app/Contents/environment/tools/img-converter/darwin/img-converter -p /Users/ranqiyu/GUI-Guider-Projects/papl_demo_big/import/faceBackground.png -n images/_faceBackground_720x1440 -w 720 -h 1440 -f true-color-alpha -d 24 Error: Run into trouble to generate picture C file&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How fix it?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 14 Aug 2022 14:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1505855#M131</guid>
      <dc:creator>lucky1</dc:creator>
      <dc:date>2022-08-14T14:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: GUI-guider exception, Error: Image size out of limit. The width and height should not exceed 128</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1505988#M133</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205029"&gt;@lucky1&lt;/a&gt;, have you tried resizing the picture to have a height of 1280 or less?&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 06:00:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1505988#M133</guid>
      <dc:creator>david_piskula</dc:creator>
      <dc:date>2022-08-15T06:00:00Z</dc:date>
    </item>
    <item>
      <title>Re: GUI-guider exception, Error: Image size out of limit. The width and height should not exceed 128</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506049#M134</link>
      <description>&lt;P&gt;In fact, if resizing image widget size to have a height of 1280 or less, won't have this exception.&lt;/P&gt;&lt;P&gt;But our display resolution height exceed 1280 to 1440, the lvgl image widget needs to cover the entire display area.&lt;/P&gt;&lt;P&gt;By the way, the real resolution of the picture file is 360x720, not the lvgl image widget size .&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 07:28:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506049#M134</guid>
      <dc:creator>lucky1</dc:creator>
      <dc:date>2022-08-15T07:28:01Z</dc:date>
    </item>
    <item>
      <title>Re: GUI-guider exception, Error: Image size out of limit. The width and height should not exceed 128</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506056#M135</link>
      <description>&lt;P&gt;Hello, can you please describe your whole setup? Which MCU are you using, what are the display dimensions, how did you configure the GuiGuider project?&lt;/P&gt;
&lt;P&gt;Or are you only experimenting with the simulator for now?&lt;/P&gt;
&lt;P&gt;I am able to reproduce your issue and will report it to our developers.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 07:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506056#M135</guid>
      <dc:creator>david_piskula</dc:creator>
      <dc:date>2022-08-15T07:51:56Z</dc:date>
    </item>
    <item>
      <title>Re: GUI-guider exception, Error: Image size out of limit. The width and height should not exceed 128</title>
      <link>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506161#M138</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/205029"&gt;@lucky1&lt;/a&gt;, this is a bug in the tool probably made from the assumption that only the officially supported displays (with 1280 px max size) would be supported. The limitation will be removed in version 1.4.1 so that displays of any size can be supported properly. For now a workaround would be to split the image into two parts and create two image widgets.&lt;/P&gt;
&lt;P&gt;Thank you for reporting this issue.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 12:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/GUI-guider-exception-Error-Image-size-out-of-limit-The-width-and/m-p/1506161#M138</guid>
      <dc:creator>david_piskula</dc:creator>
      <dc:date>2022-08-15T12:07:25Z</dc:date>
    </item>
  </channel>
</rss>