<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI Guiderのトピック回复： Gui Guider V1.9.0 Create Project Issue</title>
    <link>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2043137#M1337</link>
    <description>&lt;P&gt;I also have the same problem, unable to create a project,popup error message"Download is failed, please check your network"&lt;/P&gt;&lt;P&gt;i tryed for turned off The firewall or Add Gui-Guider.exe to the trusted application list of the firewall, The problem still occurs&lt;/P&gt;</description>
    <pubDate>Thu, 13 Feb 2025 06:27:01 GMT</pubDate>
    <dc:creator>sjg</dc:creator>
    <dc:date>2025-02-13T06:27:01Z</dc:date>
    <item>
      <title>Gui Guider V1.9.0 Create Project Issue</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2037732#M1326</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have recently installed Gui Guider V1.9.0 on my work laptop which is running Windows 11. When creating a new project, using LVGL v8.3.10 or v9.2.1, I receive an error message when I press the &amp;lt;CREATE&amp;gt; button. The message states "download is failed; check your network". A colleague has also experienced this on his workstation.&lt;/P&gt;&lt;P&gt;Please see the Device Specifications of my Windows machine:&lt;/P&gt;&lt;P&gt;OS: Windows 11 Enterprise (64-bit)&lt;/P&gt;&lt;P&gt;Version: 23H2&lt;/P&gt;&lt;P&gt;CPU: Intel i7-11850H&lt;/P&gt;&lt;P&gt;RAM: 64GB&lt;/P&gt;&lt;P&gt;Any suggestions are greatly appreciated.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tony Belehradek&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 14:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2037732#M1326</guid>
      <dc:creator>tony_belehradek</dc:creator>
      <dc:date>2025-02-04T14:17:32Z</dc:date>
    </item>
    <item>
      <title>Re: Gui Guider V1.9.0 Create Project Issue</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2037992#M1327</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/177003"&gt;@tony_belehradek&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please try disabling firewall protection, or enabling public network access to GUI Guider via the firewall.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 20:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2037992#M1327</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-02-04T20:24:54Z</dc:date>
    </item>
    <item>
      <title>回复： Gui Guider V1.9.0 Create Project Issue</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2043137#M1337</link>
      <description>&lt;P&gt;I also have the same problem, unable to create a project,popup error message"Download is failed, please check your network"&lt;/P&gt;&lt;P&gt;i tryed for turned off The firewall or Add Gui-Guider.exe to the trusted application list of the firewall, The problem still occurs&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 06:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2043137#M1337</guid>
      <dc:creator>sjg</dc:creator>
      <dc:date>2025-02-13T06:27:01Z</dc:date>
    </item>
    <item>
      <title>回复： Gui Guider V1.9.0 Create Project Issue</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2043897#M1347</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243336"&gt;@sjg&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Have you tried on a different network? Also, are you running GUI Guider as administrator?&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 21:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2043897#M1347</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-02-13T21:21:44Z</dc:date>
    </item>
    <item>
      <title>回复： Gui Guider V1.9.0 Create Project Issue</title>
      <link>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2044074#M1349</link>
      <description>thanks! It's ok with running GUI Guider as administrator</description>
      <pubDate>Fri, 14 Feb 2025 01:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/Gui-Guider-V1-9-0-Create-Project-Issue/m-p/2044074#M1349</guid>
      <dc:creator>sjg</dc:creator>
      <dc:date>2025-02-14T01:45:05Z</dc:date>
    </item>
  </channel>
</rss>