<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI GuiderのトピックRe: getting an error message. run target or generate code</title>
    <link>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1299152#M13</link>
    <description>&lt;P&gt;Thank you for the reply. I have managed to get it working now.&lt;/P&gt;&lt;P&gt;To get it to work, I power down everything and unplug everything. Waited a few minutes, then turned on everything. And I repeated the build and download. I did your instructions on hooking everything up that’s the way I had it to begin with. I have not experienced the same problem since and haven’t able to reproduce it. There must’ve been some bad code in memory that was causing the confusion on the bord&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jun 2021 14:38:41 GMT</pubDate>
    <dc:creator>skruglewicz</dc:creator>
    <dc:date>2021-06-28T14:38:41Z</dc:date>
    <item>
      <title>getting an error message. run target or generate code</title>
      <link>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1296432#M9</link>
      <description>&lt;P&gt;when I try to run my design using the I.MXRT1170-EVK I receive the following errors?&lt;/P&gt;&lt;P&gt;What does this mean? what am I missing? I have my project incased in the SDK demo&amp;nbsp; littlevgl_guider_m7&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I also cannot debug the SDK demo? It has a simular problem I cannot debug.&lt;/P&gt;&lt;P&gt;Then error list is not complete:&lt;/P&gt;&lt;P&gt;ERROR:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[100%] Built target littlevgl_guider_cm7.elf&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ns: MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Wc(03). No cache support. Nc: Found chip XML file in C:\Users\skrug\Documents\MCUXpressoIDE_11.3.1_5262\workspace\evkmimxrt1170_littlevgl_guider_cm7_experiment1\test2\deploy\config\MIMXRT1176xxxxx.xml&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Nc: Restarted LinkServer process (PID 11448).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Nc: Reconnected to existing LinkServer process.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ns: redlink server client - failed to receive response (to op 26) from server after 2000ms - timed out (rc 138)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Nc: Server OK but no connection to probe 0 core -2(ANY) (after 3 attempts) - Ee(42). Could not connect to core. Ed:02: Failed on connect: Ee(42). Could not connect to core. Et:31: No connection to chip's debug port&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 01:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1296432#M9</guid>
      <dc:creator>skruglewicz</dc:creator>
      <dc:date>2021-06-23T01:38:52Z</dc:date>
    </item>
    <item>
      <title>Re: getting an error message. run target or generate code</title>
      <link>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1296475#M10</link>
      <description>&lt;P&gt;Hi,&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/187040" target="_self"&gt;&lt;SPAN class=""&gt;skruglewicz&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1. This log from Gui guider "Run target" function or MCuxpresso IDE Debug info?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;a) MCUx IDE version?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. Can you check your target hardware prerequisites?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;a) USB cable to connect the board with your PC via USB port J11.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;b) Connect your I.MXRT1170-EVK with the power supply.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;c) Set the mini DIP switches SW1 and SW2 to QSPI Flash boot mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;d) Power on the board using power switch SW5.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 03:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1296475#M10</guid>
      <dc:creator>LiubinGong</dc:creator>
      <dc:date>2021-06-23T03:22:57Z</dc:date>
    </item>
    <item>
      <title>Re: getting an error message. run target or generate code</title>
      <link>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1299152#M13</link>
      <description>&lt;P&gt;Thank you for the reply. I have managed to get it working now.&lt;/P&gt;&lt;P&gt;To get it to work, I power down everything and unplug everything. Waited a few minutes, then turned on everything. And I repeated the build and download. I did your instructions on hooking everything up that’s the way I had it to begin with. I have not experienced the same problem since and haven’t able to reproduce it. There must’ve been some bad code in memory that was causing the confusion on the bord&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 14:38:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/getting-an-error-message-run-target-or-generate-code/m-p/1299152#M13</guid>
      <dc:creator>skruglewicz</dc:creator>
      <dc:date>2021-06-28T14:38:41Z</dc:date>
    </item>
  </channel>
</rss>