<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>GUI GuiderのトピックRe: TCP/IP connection in gui guider</title>
    <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1893233#M1055</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Without specific information about hardware you are using, it's difficult to give detailed instructions.&amp;nbsp;Here’s a general guide to help you get started:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;1. Create a New Project in GUI Guider&lt;BR /&gt;&amp;nbsp; 1. Launch GUI Guider and create a new project.&lt;BR /&gt;&amp;nbsp; 2. Design Your GUI: Add necessary elements that will interact with the network, like buttons, text fields, etc.&lt;BR /&gt;2. Integrate Network Communication Code&lt;BR /&gt;Add Network Libraries&lt;BR /&gt;• LWIP (Lightweight IP): This is a popular TCP/IP stack for embedded systems. You can use it in a simulated environment.&lt;BR /&gt;• Simulator Setup: Configure the simulator to use a virtual network interface.&lt;BR /&gt;3. Writing Code&lt;BR /&gt;1. Initialize Network Interface: Configure the LWIP stack or similar to work with the virtual network interface.&lt;BR /&gt;2. Establish Connection: Write code to connect to a server or another client. This could be done using TCP or UDP protocols.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jun 2024 02:21:53 GMT</pubDate>
    <dc:creator>Harry_Zhang</dc:creator>
    <dc:date>2024-06-25T02:21:53Z</dc:date>
    <item>
      <title>TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1874443#M998</link>
      <description>&lt;P&gt;How to establish any communication protocol like TCP/IP to send and receive data from backend?&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 08:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1874443#M998</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-05-24T08:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1875811#M1000</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you give me more details?&lt;/P&gt;
&lt;P&gt;What does backend refer to?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 01:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1875811#M1000</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-05-28T01:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1878849#M1018</link>
      <description>&lt;P&gt;I want to establish a communication protocol between two devices. And i want it to be network connected.&lt;/P&gt;&lt;P&gt;That is the backend can some device which sends data that has to be set in the screen.&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 09:18:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1878849#M1018</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-05-31T09:18:28Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1880189#M1020</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the Gui Guider can display the transmitted and sent data.&lt;/P&gt;&lt;P&gt;Firstly, you need to enable communication between the two boards.&lt;/P&gt;&lt;P&gt;Then, you can use the widgets of the Gui Guider to bind the data that needs to be sent.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this will help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jun 2024 02:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1880189#M1020</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-04T02:08:12Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1882329#M1024</link>
      <description>&lt;P&gt;Can we establish a network-based communication?&lt;/P&gt;&lt;P&gt;The data can be sent by a server and that is to be binded by the widgets and displayed in the board. If it is possible, then can you give an idea on how to implement it.&lt;/P&gt;</description>
      <pubDate>Thu, 06 Jun 2024 04:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1882329#M1024</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-06-06T04:56:13Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1885627#M1029</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, this is possible.&lt;BR /&gt;You can first make your board capable of network communication, either via WiFi or Phy.&lt;BR /&gt;Then you can use GUI Guider to display the data transmitted through the transmission network.&lt;/P&gt;&lt;P&gt;Hope this will help you.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 02:16:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1885627#M1029</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-12T02:16:40Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1885760#M1030</link>
      <description>&lt;P&gt;Thank you so much for your input. But I still want to know how to establish the connection between the board and the gui guider IDE and how to bind the widgets with data received? Can you please share your input on this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 05:18:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1885760#M1030</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-06-12T05:18:10Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1886052#M1031</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Firstly,&amp;nbsp;you can select the board you need in Gui Guider IDE.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="HangZhang_0-1718185198916.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283686i04A2F63245E0817D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="HangZhang_0-1718185198916.png" alt="HangZhang_0-1718185198916.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;HangZhang_0-1718185198916.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Then you can add a label widgets to display the received data, and add&amp;nbsp;events.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;And&amp;nbsp; you can port network communication code in this project. You can add a timer. When the timer is interrupted, the data received by the network is displayed in the label.&lt;/P&gt;
&lt;P&gt;These are just some of my suggestions, please add features according to your specific needs.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jun 2024 10:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1886052#M1031</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-12T10:17:01Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1886960#M1032</link>
      <description>&lt;P&gt;Thank you so much for your insight. So, I tried to establish a TCP server/client communication and I'm facing an issue. The code is correct, and it runs fine. But when I integrate it with gui guider and try to run it.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VARSHA_PRIYADARSINI_0-1718276161738.jpeg" style="width: 258px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283991iD8105A5121F491CC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VARSHA_PRIYADARSINI_0-1718276161738.jpeg" alt="VARSHA_PRIYADARSINI_0-1718276161738.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;VARSHA_PRIYADARSINI_0-1718276161738.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also tried to run it in cmd, also faced a similar error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="VARSHA_PRIYADARSINI_1-1718276187404.jpeg" style="width: 550px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/283992iBF4D1C4D6FC58184/image-size/medium?v=v2&amp;amp;px=400" role="button" title="VARSHA_PRIYADARSINI_1-1718276187404.jpeg" alt="VARSHA_PRIYADARSINI_1-1718276187404.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;VARSHA_PRIYADARSINI_1-1718276187404.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know how to resolve it.&lt;/P&gt;&lt;P&gt;If possible, can you give me a sample project on how to establish it.&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229957"&gt;@Harry_Zhang&lt;/a&gt;&amp;nbsp;Would very much appreciate your help.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jun 2024 10:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1886960#M1032</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-06-13T10:57:56Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1887655#M1034</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm sorry, there's currently no project that can meet your needs.&lt;/P&gt;
&lt;P&gt;May I ask what part number you are using?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 07:47:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1887655#M1034</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-14T07:47:41Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1887765#M1035</link>
      <description>&lt;P&gt;Part number means what are you referring to?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229957"&gt;@Harry_Zhang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jun 2024 09:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1887765#M1035</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-06-14T09:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1888324#M1038</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;What I mean is which chip you are currently using? I need to record it here.&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 03:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1888324#M1038</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-17T03:00:48Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1888426#M1039</link>
      <description>&lt;P&gt;I am not using any chip. I'm trying with the simulator option.&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229957"&gt;@Harry_Zhang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 06:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1888426#M1039</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-06-17T06:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1891178#M1045</link>
      <description>&lt;P&gt;I'm still looking for a solution. I don't have any hardware, trying with the simulator in windows only. Can you please guide me to establish any network communication protocol?&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 07:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1891178#M1045</guid>
      <dc:creator>VARSHA_PRIYADARSINI</dc:creator>
      <dc:date>2024-06-20T07:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: TCP/IP connection in gui guider</title>
      <link>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1893233#M1055</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234066"&gt;@VARSHA_PRIYADARSINI&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Without specific information about hardware you are using, it's difficult to give detailed instructions.&amp;nbsp;Here’s a general guide to help you get started:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;1. Create a New Project in GUI Guider&lt;BR /&gt;&amp;nbsp; 1. Launch GUI Guider and create a new project.&lt;BR /&gt;&amp;nbsp; 2. Design Your GUI: Add necessary elements that will interact with the network, like buttons, text fields, etc.&lt;BR /&gt;2. Integrate Network Communication Code&lt;BR /&gt;Add Network Libraries&lt;BR /&gt;• LWIP (Lightweight IP): This is a popular TCP/IP stack for embedded systems. You can use it in a simulated environment.&lt;BR /&gt;• Simulator Setup: Configure the simulator to use a virtual network interface.&lt;BR /&gt;3. Writing Code&lt;BR /&gt;1. Initialize Network Interface: Configure the LWIP stack or similar to work with the virtual network interface.&lt;BR /&gt;2. Establish Connection: Write code to connect to a server or another client. This could be done using TCP or UDP protocols.&lt;/P&gt;
&lt;P&gt;Hope this will help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Hang&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 02:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/GUI-Guider/TCP-IP-connection-in-gui-guider/m-p/1893233#M1055</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2024-06-25T02:21:53Z</dc:date>
    </item>
  </channel>
</rss>