<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SE050 SCP03 Key reset in EdgeLock 2GO Secure Service</title>
    <link>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2144450#M11</link>
    <description>&lt;P&gt;Resetting SCP03 keys to factory default is generally **not possible** due to the high-security design of the protocol; a simple reset would be a major vulnerability. The only way to change these keys is through a **re-personalization process with a new set of keys**, which crucially requires successful authentication using the **current, valid SCP03 keys**. If the current keys are lost or unknown, the card becomes unmanageable for secure operations.&lt;/P&gt;</description>
    <pubDate>Thu, 31 Jul 2025 09:43:40 GMT</pubDate>
    <dc:creator>steven456a</dc:creator>
    <dc:date>2025-07-31T09:43:40Z</dc:date>
    <item>
      <title>SE050 SCP03 Key reset</title>
      <link>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2024148#M2</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was wondering if there is a way to reset the SCP03 keys back to factory default?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;with kind regards,&lt;/P&gt;&lt;P&gt;Timon Vos,&lt;/P&gt;&lt;P&gt;EAL&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jan 2025 15:27:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2024148#M2</guid>
      <dc:creator>eal-fox</dc:creator>
      <dc:date>2025-01-08T15:27:15Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 SCP03 Key reset</title>
      <link>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2024398#M3</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237989"&gt;@eal-fox&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry, but no such method to reset the&amp;nbsp;SCP03 Keys. You must have the current keys to rotate them to any new keys, otherwise it would be so easy for attackers to hack the system.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 02:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2024398#M3</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-01-09T02:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: SE050 SCP03 Key reset</title>
      <link>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2144450#M11</link>
      <description>&lt;P&gt;Resetting SCP03 keys to factory default is generally **not possible** due to the high-security design of the protocol; a simple reset would be a major vulnerability. The only way to change these keys is through a **re-personalization process with a new set of keys**, which crucially requires successful authentication using the **current, valid SCP03 keys**. If the current keys are lost or unknown, the card becomes unmanageable for secure operations.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Jul 2025 09:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/EdgeLock-2GO-Secure-Service/SE050-SCP03-Key-reset/m-p/2144450#M11</guid>
      <dc:creator>steven456a</dc:creator>
      <dc:date>2025-07-31T09:43:40Z</dc:date>
    </item>
  </channel>
</rss>