<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cannot connect to taget with RESET (pin 15) high, but shoud be low in Hardware</title>
    <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1913633#M35</link>
    <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fail1" style="width: 615px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289560i5621BFB98D8F380C/image-size/large?v=v2&amp;amp;px=999" role="button" title="JTAG fail.png" alt="fail1" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fail1&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fail2" style="width: 589px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289561i7D3627841434D8A1/image-size/large?v=v2&amp;amp;px=999" role="button" title="SWD fail.png" alt="fail2" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fail2&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;It's the same whether it's SWD or JTAG. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is there another method I can consider?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Jul 2024 05:20:14 GMT</pubDate>
    <dc:creator>TnseoRnr</dc:creator>
    <dc:date>2024-07-22T05:20:14Z</dc:date>
    <item>
      <title>Cannot connect to taget with RESET (pin 15) high, but shoud be low</title>
      <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1905958#M27</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;We have a custom board that is very similar to the EVB. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I was using it well, but suddenly a problem arose for no reason. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am using Jlink. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am trying to connect using JFlash, MCUXpresso IDE, JLINK.exe (command window?), but it fails. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;On multiple identical boards, only certain boards exhibit this symptom. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;As expected, I am wondering if a hardware issue has occurred in the IC or MCU, or if protection such as protection mode is in progress. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Below is the message that occurs when attempting a JLINK connection.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;*JLINK.exe&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Connecting to target via JTAG&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Failed to identify target. Resetting via Reset pin and trying again.&lt;BR /&gt;RESET (pin 15) high, but should be low. Please check target hardware.&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Failed to identify target. Resetting via Reset pin and trying again.&lt;BR /&gt;RESET (pin 15) high, but should be low. Please check target hardware.&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Cannot connect to target.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Even on boards where JLINK connection is difficult, the last downloaded firmware is operating normally.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;The key is that I used the firmware update normally and then it became unusable. &lt;/SPAN&gt;&lt;SPAN class=""&gt;Other identical boards are still being used while updating their firmware normally.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;The MCU is using MIMXRT1176XXXA_M7 and referenced MIMXRT1170-EVK. The JTAG-related circuit is used almost similarly to the EVB board.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;What can I check?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jul 2024 07:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1905958#M27</guid>
      <dc:creator>TnseoRnr</dc:creator>
      <dc:date>2024-07-11T07:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to taget with RESET (pin 15) high, but shoud be low</title>
      <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1908214#M29</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231615"&gt;@TnseoRnr&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Do you connect the JTAG_MOD pin to the ground or not?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1721013180546.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288474iB976D6BC759C7AF8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1721013180546.png" alt="kerryzhou_0-1721013180546.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you also try the SWD interface, whether that works or not?&lt;/P&gt;
&lt;P&gt;You can use the JLINK commander to connect, and share the whole log.&lt;/P&gt;
&lt;P&gt;From your test result, should still related to your board hardware, as some board works with the same schematic, maybe you also need to check the power on sequence, whether the power is correct or not.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 03:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1908214#M29</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-07-15T03:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to taget with RESET (pin 15) high, but shoud be low</title>
      <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1910136#M30</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Yes, it is grounded. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Again, I have the same model in good use. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;My guess is that it is protected or the MCU is damaged, but the previously downloaded firmware operates normally even in the MCU where JTAG is not connected. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is there anything I can check?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 00:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1910136#M30</guid>
      <dc:creator>TnseoRnr</dc:creator>
      <dc:date>2024-07-17T00:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to taget with RESET (pin 15) high, but shoud be low</title>
      <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1910440#M31</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231615"&gt;@TnseoRnr&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; You mean, the same board schematic, more boards, some board is working, just some board is not working, right?&lt;/P&gt;
&lt;P&gt;&amp;nbsp; If this situation, use the JILNK commander to check your chip, whether can find the ARM core or not, if can't find the ARM core, it means your hardware solder may have issues.&lt;/P&gt;
&lt;P&gt;I mean, something like this:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kerryzhou_0-1721205796624.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/288925i69FC049B48BB593E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kerryzhou_0-1721205796624.jpeg" alt="kerryzhou_0-1721205796624.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 08:43:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1910440#M31</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-07-17T08:43:26Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to taget with RESET (pin 15) high, but shoud be low</title>
      <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1913633#M35</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fail1" style="width: 615px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289560i5621BFB98D8F380C/image-size/large?v=v2&amp;amp;px=999" role="button" title="JTAG fail.png" alt="fail1" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fail1&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fail2" style="width: 589px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/289561i7D3627841434D8A1/image-size/large?v=v2&amp;amp;px=999" role="button" title="SWD fail.png" alt="fail2" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fail2&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;It's the same whether it's SWD or JTAG. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is there another method I can consider?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 05:20:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1913633#M35</guid>
      <dc:creator>TnseoRnr</dc:creator>
      <dc:date>2024-07-22T05:20:14Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot connect to taget with RESET (pin 15) high, but shoud be low</title>
      <link>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1914742#M36</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231615"&gt;@TnseoRnr&lt;/a&gt;&amp;nbsp;，&lt;/P&gt;
&lt;P&gt;&amp;nbsp; Thanks for your updated information.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; JLINK can't find your ARM core, it means your hardware still have issues, you need to check your customer hardware situation, the power on sequence, etc.&lt;/P&gt;
&lt;P&gt;Please double check your hardware at first, thanks.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jul 2024 07:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Cannot-connect-to-taget-with-RESET-pin-15-high-but-shoud-be-low/m-p/1914742#M36</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2024-07-23T07:02:58Z</dc:date>
    </item>
  </channel>
</rss>