<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>HardwareのトピックVL82C420 Datasheet missing</title>
    <link>https://community.nxp.com/t5/Hardware/VL82C420-Datasheet-missing/m-p/2058250#M113</link>
    <description>&lt;P&gt;I’m seeking information pertaining to the above VLSI chipset&lt;/P&gt;&lt;P&gt;i’ve searched the web to find details of the pin connections and this was used in &amp;nbsp;number of notebooks using the 486SL CPU&lt;/P&gt;&lt;P&gt;It was part of the SCAMP IV Chipset&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;VLSI Technology’s notebook chips include the 82C420 System Controller, 82C144 Peripheral Controller, 82C146 PCMCIA&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Controller, and the 82C170 LCD Graphics Accelerator. VLSI’s ML Bus is time-multiplexed onto the low 16 bits of the local bus.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I am knocking every door to find the datasheet for the VL82C420&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;It is known the chip was used in the following notebooks in the 90’s&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;AST Ascentia 910N&lt;BR /&gt;Compaq Lte Elite 4/50CX, 4/75C, 75CX, 75CX&lt;BR /&gt;IBM Thinkpad 230Cs&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;IBM Palmtop PC110&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;If anyone has the datasheet or pinout then please contact me.&lt;/P&gt;&lt;P class=""&gt;Thanks Mike&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 08 Mar 2025 22:36:07 GMT</pubDate>
    <dc:creator>Mike1978uk</dc:creator>
    <dc:date>2025-03-08T22:36:07Z</dc:date>
    <item>
      <title>VL82C420 Datasheet missing</title>
      <link>https://community.nxp.com/t5/Hardware/VL82C420-Datasheet-missing/m-p/2058250#M113</link>
      <description>&lt;P&gt;I’m seeking information pertaining to the above VLSI chipset&lt;/P&gt;&lt;P&gt;i’ve searched the web to find details of the pin connections and this was used in &amp;nbsp;number of notebooks using the 486SL CPU&lt;/P&gt;&lt;P&gt;It was part of the SCAMP IV Chipset&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;VLSI Technology’s notebook chips include the 82C420 System Controller, 82C144 Peripheral Controller, 82C146 PCMCIA&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Controller, and the 82C170 LCD Graphics Accelerator. VLSI’s ML Bus is time-multiplexed onto the low 16 bits of the local bus.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I am knocking every door to find the datasheet for the VL82C420&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;It is known the chip was used in the following notebooks in the 90’s&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;AST Ascentia 910N&lt;BR /&gt;Compaq Lte Elite 4/50CX, 4/75C, 75CX, 75CX&lt;BR /&gt;IBM Thinkpad 230Cs&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;IBM Palmtop PC110&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;If anyone has the datasheet or pinout then please contact me.&lt;/P&gt;&lt;P class=""&gt;Thanks Mike&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 08 Mar 2025 22:36:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/VL82C420-Datasheet-missing/m-p/2058250#M113</guid>
      <dc:creator>Mike1978uk</dc:creator>
      <dc:date>2025-03-08T22:36:07Z</dc:date>
    </item>
    <item>
      <title>Re: VL82C420 Datasheet missing</title>
      <link>https://community.nxp.com/t5/Hardware/VL82C420-Datasheet-missing/m-p/2088535#M118</link>
      <description>&lt;P&gt;I've also been trying to find the data-sheet for the VL82C420. Appreciate it's before NXP's time but hopefully it's in a vault somewhere, it would be immensely helpful to have it.&lt;/P&gt;&lt;P&gt;Cheers, Nick.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Apr 2025 15:21:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/VL82C420-Datasheet-missing/m-p/2088535#M118</guid>
      <dc:creator>zikolas</dc:creator>
      <dc:date>2025-04-28T15:21:47Z</dc:date>
    </item>
  </channel>
</rss>