<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>HardwareのトピックIs an external clock generator required when using SerDes in the S32Gx Familly?</title>
    <link>https://community.nxp.com/t5/Hardware/Is-an-external-clock-generator-required-when-using-SerDes-in-the/m-p/2039911#M107</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi, all&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When designing circuits with the S32Gx Family, is an external clock generator required for using SerDes?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am curious if it is possible to use only the internal PLL without an external clock generator.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks and best regards&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Feb 2025 10:46:59 GMT</pubDate>
    <dc:creator>Ralph88</dc:creator>
    <dc:date>2025-02-07T10:46:59Z</dc:date>
    <item>
      <title>Is an external clock generator required when using SerDes in the S32Gx Familly?</title>
      <link>https://community.nxp.com/t5/Hardware/Is-an-external-clock-generator-required-when-using-SerDes-in-the/m-p/2039911#M107</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, all&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;When designing circuits with the S32Gx Family, is an external clock generator required for using SerDes?&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am curious if it is possible to use only the internal PLL without an external clock generator.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks and best regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 10:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Is-an-external-clock-generator-required-when-using-SerDes-in-the/m-p/2039911#M107</guid>
      <dc:creator>Ralph88</dc:creator>
      <dc:date>2025-02-07T10:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: Is an external clock generator required when using SerDes in the S32Gx Familly?</title>
      <link>https://community.nxp.com/t5/Hardware/Is-an-external-clock-generator-required-when-using-SerDes-in-the/m-p/2039983#M108</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246543"&gt;@Ralph88&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;An external reference clock is required which meets PCIe Gen3 clock specifications.&lt;/P&gt;
&lt;P&gt;If PCIe Gen3 is not required in your design, The internal reference clock can be used for supporting PCIe Gen2 and SGMII communication.&lt;/P&gt;
&lt;P&gt;I hope it will help.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 13:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Hardware/Is-an-external-clock-generator-required-when-using-SerDes-in-the/m-p/2039983#M108</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-02-07T13:08:07Z</dc:date>
    </item>
  </channel>
</rss>