<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMC9S08QG8  RTI frquency trim</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126225#M990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I need the MC9S08QG8 RTI to keep time (count seconds) when it is running and also in stop3 mode. I have no problems doing this, however, I cant seem to trim the frequency. It appears the 1KHz RTI oscilator is independant of the internal reference oscilator. Am I right?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If this is the case, I can RTI every 8ms and count down 125 to increment seconds. By changing the counter preset (125) up or down I will&amp;nbsp;able to trim&amp;nbsp;for accuracy. My question is: How stable is this oscilator when it comes to temperature or PSU changes? I see no information in the data sheet for this oscilator, only for the ICS clock reference.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 11 Feb 2006 08:19:20 GMT</pubDate>
    <dc:creator>paul</dc:creator>
    <dc:date>2006-02-11T08:19:20Z</dc:date>
    <item>
      <title>MC9S08QG8  RTI frquency trim</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126225#M990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I need the MC9S08QG8 RTI to keep time (count seconds) when it is running and also in stop3 mode. I have no problems doing this, however, I cant seem to trim the frequency. It appears the 1KHz RTI oscilator is independant of the internal reference oscilator. Am I right?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If this is the case, I can RTI every 8ms and count down 125 to increment seconds. By changing the counter preset (125) up or down I will&amp;nbsp;able to trim&amp;nbsp;for accuracy. My question is: How stable is this oscilator when it comes to temperature or PSU changes? I see no information in the data sheet for this oscilator, only for the ICS clock reference.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Feb 2006 08:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126225#M990</guid>
      <dc:creator>paul</dc:creator>
      <dc:date>2006-02-11T08:19:20Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8  RTI frquency trim</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126226#M991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;The accuracy of this clock is quoted as +/- 30% so I couldn't imagine its stability would be too brilliant.&lt;/P&gt;&lt;P&gt;Peg&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Feb 2006 15:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126226#M991</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-02-11T15:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8  RTI frquency trim</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126227#M992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;The specs also state that the DCO could be between 25Khz and 41KHz (32.7KHz typ), but once trimmed, will remain +/- 0.5% from 0 to 70 degrees C. I consider that quite stable for no crystal.&lt;/P&gt;&lt;P&gt;Would&amp;nbsp;the accuracy&amp;nbsp;be the same for RTI oscilator?&lt;/P&gt;&lt;P&gt;Has anyone used this MCU's internal clock source for real time clock purposes?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Feb 2006 00:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126227#M992</guid>
      <dc:creator>paul</dc:creator>
      <dc:date>2006-02-12T00:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8  RTI frquency trim</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126228#M993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Hi Paul,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;I wouldn't expect the RTI clock to be very precise.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Principal reason is that the RTI would be used to wake the MCU up every so often for it to analyze and see if there is something to do.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;As the power consumption is important there, that will be an RC oscillator just for the RTI module.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Actually it will be precise on one MCU and won't vary a lot&amp;nbsp;at&amp;nbsp;a given&amp;nbsp;temperature. But the next MCU will be different because of the fab process and no characterization done on it.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Cheers,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Comic Sans MS"&gt;Alban.&lt;/FONT&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2006 23:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126228#M993</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-02-15T23:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08QG8  RTI frquency trim</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126229#M994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT face="Comic Sans MS"&gt;Yep Peg,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Comic Sans MS"&gt;I would see a typical 25% for this kind of&amp;nbsp;really simple RC-oscillators.&lt;BR /&gt;The 30% is probably quoted with some guard band to guarantee it across production.&lt;BR /&gt;&lt;BR /&gt;Alban.&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2006 23:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08QG8-RTI-frquency-trim/m-p/126229#M994</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2006-02-15T23:46:37Z</dc:date>
    </item>
  </channel>
</rss>