<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Problems with CodeWarrior Chip Emulation and MC68HC908QT4 AWU</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161581#M9818</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have never tested it, but it would not surprise me that stop mode, and therefore AWU operation,&amp;nbsp;would not be simulated under FCS.&amp;nbsp; If this is so, I would&amp;nbsp;assume that the stop instruction would be ignored, and the simulated execution would continue with the following instruction.&amp;nbsp; Is this what you have observed?&amp;nbsp; However, I would expect that an interrupt for the associated timer would be simulated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As far as I can see, little would be gained by simulating stop mode - this ultimately needs to be tested on the actual hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Nov 2010 00:30:29 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-11-11T00:30:29Z</dc:date>
    <item>
      <title>Problems with CodeWarrior Chip Emulation and MC68HC908QT4 AWU</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161579#M9816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, as described in the subject I have some problems getting the Auto Wark Up working for my HC908QT4. I checked if the AWUIE is enabled, and it is. Nevertheless my generated method is never been called after the MCU enters the stop mode. Any suggestions what i'm doing wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards Wolf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Using Version 5.9.0 Build 5292 of CodeWarrior&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Nov 2010 01:01:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161579#M9816</guid>
      <dc:creator>F_Wolf</dc:creator>
      <dc:date>2010-11-10T01:01:39Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with CodeWarrior Chip Emulation and MC68HC908QT4 AWU</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161580#M9817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The CW i have installed is 6.3.1 the 5.9 mentioned above is from the about Tab of CW, the 6.3 from the installer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But to fromulate my question more general:&lt;/P&gt;&lt;P&gt;Is the AWU functionality in general implemented in CW? I have the feeling it is not.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Wolf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for writing a new post, but editing the old seems not permitted anymore.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Nov 2010 20:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161580#M9817</guid>
      <dc:creator>F_Wolf</dc:creator>
      <dc:date>2010-11-10T20:59:04Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with CodeWarrior Chip Emulation and MC68HC908QT4 AWU</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161581#M9818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have never tested it, but it would not surprise me that stop mode, and therefore AWU operation,&amp;nbsp;would not be simulated under FCS.&amp;nbsp; If this is so, I would&amp;nbsp;assume that the stop instruction would be ignored, and the simulated execution would continue with the following instruction.&amp;nbsp; Is this what you have observed?&amp;nbsp; However, I would expect that an interrupt for the associated timer would be simulated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As far as I can see, little would be gained by simulating stop mode - this ultimately needs to be tested on the actual hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Nov 2010 00:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161581#M9818</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-11-11T00:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with CodeWarrior Chip Emulation and MC68HC908QT4 AWU</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161582#M9819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;executing the STOP instruction in the FCS will halt the CPU and it don't seem that an interrupt is generated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But maybe my configuration of the chip is wrong so that this leads to the described problem?&lt;/P&gt;&lt;P&gt;my setting is&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CONFIG1: COPRS=0,LVISTOP=1,LVIRSTD=0,LVIPWRD=0,LVI5OR3=1,SSREC=0,STOP=1,COPD=1&lt;/P&gt;&lt;P&gt;CONFIG2: IRQPUD=0,IRQEN=0,??=0,OSCOPT1=0,OSCOPT0=0,??=0,??=0,RSTEN=0&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;PTA: PTA5=0,PTA4=0,PTA3=0,PTA1=0&lt;BR /&gt;&amp;nbsp;PTAPUE: OSC2EN=0,PTAPUE5=0,PTAPUE4=0,PTAPUE3=0,PTAPUE1=0&lt;BR /&gt;&amp;nbsp;DDRA: DDRA5=1,DDRA4=1,DDRA3=1,DDRA1=1,DDRA0=0&lt;BR /&gt;&amp;nbsp;KBIER: AWUIE=1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;KBSCR: ACKK=1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Nov 2010 04:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-CodeWarrior-Chip-Emulation-and-MC68HC908QT4-AWU/m-p/161582#M9819</guid>
      <dc:creator>F_Wolf</dc:creator>
      <dc:date>2010-11-11T04:28:30Z</dc:date>
    </item>
  </channel>
</rss>