<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unable to erase the flash on a GT16A in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160991#M9734</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response Peg.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes&amp;nbsp;I&amp;nbsp;can connect to the device (and read the System Device ID registers) but can not erase or program the device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is a new device and the programmer software reports that it is unsecured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both the programmer and debugger read NVOPT as $FE.&lt;/P&gt;&lt;P&gt;The programmer reads FOPT as $C2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are 4 bytes which are not erased:&lt;/P&gt;&lt;P&gt;$FFBE = $73&lt;/P&gt;&lt;P&gt;$FFBF = $FE&lt;/P&gt;&lt;P&gt;$FFFE = $00&lt;/P&gt;&lt;P&gt;$FFFF = $80&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The difference I have seen between the the two boards is the bus frequency reported by the programmer.&lt;/P&gt;&lt;P&gt;We use the GT16A on the old board and do not have this problem.&amp;nbsp; There is something different with this board or maybe this individual device is damaged.&amp;nbsp; I am trying to get the device swapped but I think the tool is not working.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Dec 2009 23:03:07 GMT</pubDate>
    <dc:creator>Hawkeye</dc:creator>
    <dc:date>2009-12-14T23:03:07Z</dc:date>
    <item>
      <title>Unable to erase the flash on a GT16A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160989#M9732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;I can not erase the flash when using PROGHCS08 v1.40.&amp;nbsp;&lt;/SPAN&gt; &lt;SPAN&gt;Typically it re-initializes when I choose to erase the module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The problem is with our board which we have modified. With the old board I have no problems but with the new one it fails. The changes on the board are not supposed to impact the MCU but obviously they do.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;One difference I see when attempting erase the flash is that with our new board and v1.04 of the algorithm the programmer reports a bus frequency of 7741 KHz. With an older version of the algorithm it was reporting a bus frequency of 3685 KHz. With a working board the bus frequency is reported as 15546 KHz.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can anybody suggest why the frequency is different or what to look at to solve this problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Dec 2009 05:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160989#M9732</guid>
      <dc:creator>Hawkeye</dc:creator>
      <dc:date>2009-12-12T05:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to erase the flash on a GT16A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160990#M9733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hawkeye,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you saying you can connect to the device with out any problem but only get a problem with the erase command?&lt;/P&gt;&lt;P&gt;Are you securing the device previously?&lt;/P&gt;&lt;P&gt;I use the GT16A a lot and have not seen any problem like this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Dec 2009 06:10:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160990#M9733</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-12-12T06:10:31Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to erase the flash on a GT16A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160991#M9734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the response Peg.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes&amp;nbsp;I&amp;nbsp;can connect to the device (and read the System Device ID registers) but can not erase or program the device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is a new device and the programmer software reports that it is unsecured.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both the programmer and debugger read NVOPT as $FE.&lt;/P&gt;&lt;P&gt;The programmer reads FOPT as $C2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are 4 bytes which are not erased:&lt;/P&gt;&lt;P&gt;$FFBE = $73&lt;/P&gt;&lt;P&gt;$FFBF = $FE&lt;/P&gt;&lt;P&gt;$FFFE = $00&lt;/P&gt;&lt;P&gt;$FFFF = $80&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The difference I have seen between the the two boards is the bus frequency reported by the programmer.&lt;/P&gt;&lt;P&gt;We use the GT16A on the old board and do not have this problem.&amp;nbsp; There is something different with this board or maybe this individual device is damaged.&amp;nbsp; I am trying to get the device swapped but I think the tool is not working.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Dec 2009 23:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160991#M9734</guid>
      <dc:creator>Hawkeye</dc:creator>
      <dc:date>2009-12-14T23:03:07Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to erase the flash on a GT16A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160992#M9735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe I am not really "connected" to the GT16A as the programmer always initializes and loads the programming algorithm when I select Erase Module.&lt;/P&gt;&lt;P&gt;Can anybody tell me why it would do that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Dec 2009 03:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160992#M9735</guid>
      <dc:creator>Hawkeye</dc:creator>
      <dc:date>2009-12-15T03:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to erase the flash on a GT16A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160993#M9736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Replacing the mcu solved the problem.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Dec 2009 22:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-erase-the-flash-on-a-GT16A/m-p/160993#M9736</guid>
      <dc:creator>Hawkeye</dc:creator>
      <dc:date>2009-12-24T22:14:40Z</dc:date>
    </item>
  </channel>
</rss>