<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックProgramming QB8 controller using P&amp;E micro USB multilink MONO8 connector</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-QB8-controller-using-P-E-micro-USB-multilink-MONO8/m-p/126182#M972</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm using MC68HC08QB8 processor.Not able to program the board. The programmer is USB Multilink from P&amp;amp;E micro it has a MONO8 programming 16 pin connector . When I connect the target board the yellow LED in the Programmer doesn't glow, only the blue LED glows.&lt;BR /&gt;The connector pin details:&lt;BR /&gt;Pin no. 1,3,5,7,9,11,14,16 --&amp;gt; NC,&lt;BR /&gt;&amp;nbsp;2 --&amp;gt; Gnd, 4--&amp;gt;RST (Pulled upto VCC),6--&amp;gt;IRQ(Pulled up to VCC),8--&amp;gt;PTA0, 10--&amp;gt;PTA4,12--&amp;gt;PTA1,13--&amp;gt;PTA7(pulled to VCC),15--&amp;gt; VCC.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Aug 2006 12:44:05 GMT</pubDate>
    <dc:creator>ram</dc:creator>
    <dc:date>2006-08-10T12:44:05Z</dc:date>
    <item>
      <title>Programming QB8 controller using P&amp;E micro USB multilink MONO8 connector</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-QB8-controller-using-P-E-micro-USB-multilink-MONO8/m-p/126182#M972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm using MC68HC08QB8 processor.Not able to program the board. The programmer is USB Multilink from P&amp;amp;E micro it has a MONO8 programming 16 pin connector . When I connect the target board the yellow LED in the Programmer doesn't glow, only the blue LED glows.&lt;BR /&gt;The connector pin details:&lt;BR /&gt;Pin no. 1,3,5,7,9,11,14,16 --&amp;gt; NC,&lt;BR /&gt;&amp;nbsp;2 --&amp;gt; Gnd, 4--&amp;gt;RST (Pulled upto VCC),6--&amp;gt;IRQ(Pulled up to VCC),8--&amp;gt;PTA0, 10--&amp;gt;PTA4,12--&amp;gt;PTA1,13--&amp;gt;PTA7(pulled to VCC),15--&amp;gt; VCC.&lt;BR /&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2006 12:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-QB8-controller-using-P-E-micro-USB-multilink-MONO8/m-p/126182#M972</guid>
      <dc:creator>ram</dc:creator>
      <dc:date>2006-08-10T12:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: Programming QB8 controller using P&amp;E micro USB multilink MONO8 connector</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-QB8-controller-using-P-E-micro-USB-multilink-MONO8/m-p/126183#M973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi ram,&lt;/P&gt;&lt;P&gt;The yellow LED indicates that you have power on the target board!&lt;/P&gt;&lt;P&gt;So do you? Between MON08 pins 2 &amp;amp; 15&lt;/P&gt;&lt;P&gt;Regards David&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2006 14:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-QB8-controller-using-P-E-micro-USB-multilink-MONO8/m-p/126183#M973</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2006-08-10T14:17:45Z</dc:date>
    </item>
  </channel>
</rss>