<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MC9S08SL8CTL  Inernal Bus Clock? / Trim?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160685#M9695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the LIN module is so critical, I would tend to simplify the setup.&amp;nbsp; I might choose an internal reference trim frequency of 38.0 kHz.&amp;nbsp; This will produce a bus frequency of 19.46 MHz, (i.e. nominally 2.7 percent below the maximum allowable frequency).&amp;nbsp; This will easily allow for the initial trim error, plus worst case&amp;nbsp;drift due to temperature and voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There would seem little point in expressing&amp;nbsp;the nominal trim frequency to a&amp;nbsp;precision less&amp;nbsp;than 50 or 100 Hz because of the possible&amp;nbsp;initial trim error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Nov 2010 11:13:26 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-11-08T11:13:26Z</dc:date>
    <item>
      <title>MC9S08SL8CTL  Inernal Bus Clock? / Trim?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160682#M9692</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I&amp;nbsp;needs to trim the internal reference clock in order to generate&amp;nbsp;exactly 20MHz Frequency. (and not greater than 20Mhz)&lt;/P&gt;&lt;P&gt;The problem: I become three frequency 20026178Hz , 19921875Hz and 19818652Hz after every Reset.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My internal Oscillator frequency is 390625 kHz.&lt;/P&gt;&lt;P&gt;The Trim Control at the Code Warior connection Manager is 39062,50 Hz&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The 9S08SL8CTL Internal Reference Clock&amp;nbsp;has a&amp;nbsp;accuracy of up to +/- 0.2%, so the&amp;nbsp;Internal ferequency&amp;nbsp;schould be max 20020000Hz and min 19980000Hz ???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;are there some other configuration?&lt;/P&gt;&lt;P&gt;what can I do to become a frequency equal and not greater than 20Mhz?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Nov 2010 21:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160682#M9692</guid>
      <dc:creator>kazbi</dc:creator>
      <dc:date>2010-11-04T21:33:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SL8CTL  Inernal Bus Clock? / Trim?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160683#M9693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not sure what the three different frequencies that you list represent, and how these frequencies are actually measured, and over what measurement&amp;nbsp;period.&amp;nbsp; Keep in mind that, when the FLL is utilised, its output will have a substantial amount of short term jitter, as is the nature of FLL operation.&amp;nbsp; As the time period over which the frequency measurement occurs is increased, the amount of jitter will steadily reduce.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The small frequency variations that you indicated should not be a problem for the MCU.&amp;nbsp; The potential variation of reference oscillator frequency, with change of operating temperature, is likely to be considerably greater.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If slightly exceeding the specified&amp;nbsp;upper bus frequency limit is of concern, you might consider a reduced trim frequency for the internal reference.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Nov 2010 11:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160683#M9693</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-11-05T11:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SL8CTL  Inernal Bus Clock? / Trim?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160684#M9694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Big Mac,&lt;/P&gt;&lt;P&gt;Thank you for reply : )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The real problem in my system is&amp;nbsp;the LIN communication.&lt;/P&gt;&lt;P&gt;The LIN Communication can be disabled with a frequency over 20MHz ==&amp;gt; 20,026178MHz (20Mhz +~ 0,2%(jitter)) + (2% over voltage and temperature)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I will work with a max 19569471,62Hz frequency so that the frequency in worst case don´t exceed 20Mhz&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Nov 2010 15:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160684#M9694</guid>
      <dc:creator>kazbi</dc:creator>
      <dc:date>2010-11-05T15:37:22Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SL8CTL  Inernal Bus Clock? / Trim?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160685#M9695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the LIN module is so critical, I would tend to simplify the setup.&amp;nbsp; I might choose an internal reference trim frequency of 38.0 kHz.&amp;nbsp; This will produce a bus frequency of 19.46 MHz, (i.e. nominally 2.7 percent below the maximum allowable frequency).&amp;nbsp; This will easily allow for the initial trim error, plus worst case&amp;nbsp;drift due to temperature and voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There would seem little point in expressing&amp;nbsp;the nominal trim frequency to a&amp;nbsp;precision less&amp;nbsp;than 50 or 100 Hz because of the possible&amp;nbsp;initial trim error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Nov 2010 11:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SL8CTL-Inernal-Bus-Clock-Trim/m-p/160685#M9695</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-11-08T11:13:26Z</dc:date>
    </item>
  </channel>
</rss>