<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピック&amp;quot;This limited version allows only 1024 bytes of C++ code&amp;quot; - problem with Codewarrior</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160559#M9673</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I installed evalluation version of Codewarrior from this page:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Foverview.jsp%3Fcode%3DCW_EVALS" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_EVALS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but I still have get a message which is in subject of this topic. I tried to re-install CW - no result. What more - the file that i downloaded is "CW_MCU_V6_3_EVAL" so I understand that it is version 6.3. But after installation in help menu in CW there is written Version 5.9.0&lt;/P&gt;&lt;P&gt;Please help me with my problem, my email address in registration info is valid.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 May 2012 07:04:22 GMT</pubDate>
    <dc:creator>krzy90</dc:creator>
    <dc:date>2012-05-08T07:04:22Z</dc:date>
    <item>
      <title>"This limited version allows only 1024 bytes of C++ code" - problem with Codewarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160559#M9673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I installed evalluation version of Codewarrior from this page:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Foverview.jsp%3Fcode%3DCW_EVALS" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_EVALS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but I still have get a message which is in subject of this topic. I tried to re-install CW - no result. What more - the file that i downloaded is "CW_MCU_V6_3_EVAL" so I understand that it is version 6.3. But after installation in help menu in CW there is written Version 5.9.0&lt;/P&gt;&lt;P&gt;Please help me with my problem, my email address in registration info is valid.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2012 07:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160559#M9673</guid>
      <dc:creator>krzy90</dc:creator>
      <dc:date>2012-05-08T07:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: "This limited version allows only 1024 bytes of C++ code" - problem with Codewarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160560#M9674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The special edition licence for Code Warrior has this limit for C++ code.&amp;nbsp; To extend beyond this limit you will need to purchase a suitable licence.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, the licence that you have will handle up to 32K of compiled C code, for MC9S08 MCUs.&amp;nbsp; You will need to specify that you are using C when creating a project using the new project wizard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The version number that you refer is that for the IDE program, and not the compiler, etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2012 09:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160560#M9674</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-05-08T09:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: "This limited version allows only 1024 bytes of C++ code" - problem with Codewarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160561#M9675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also, there are very few reasons why one would even consider C++ for HCS08. Special compatibility requirements etc. There are so few of the C++-specific features you can use/that makes sense to use, so you would basically end up with C anyway.&amp;nbsp; For a brand new, stand-alone HCS08 project I see no reasons whatsoever to use C++.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 May 2012 14:51:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/quot-This-limited-version-allows-only-1024-bytes-of-C-code-quot/m-p/160561#M9675</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2012-05-08T14:51:05Z</dc:date>
    </item>
  </channel>
</rss>